Skip to main content
Associate II
May 10, 2024 1:12 PM UTC
Solved

AI Road State Monitoring with AEK-MCU-C4ML1T1, AEK-CON-SENSOR1+MEMS SENSOR BOARD,AEK-LCD-DT028V1

Hi ,

We have an AEK-MCU-C4ML1T1 Discovery board. We want to simulate AI road state monitoring with AEK-CON-SENSOR1+MEMS SENSOR BOARD and AEK-LCD-DT028V1. Where do we get the complete firmware to build an application with all the features as shown in the STMicroelectronics website video(NORMAL, PARKING, BUMPY SKID)? 

What are the tools required to build a complete application?

How can we get CPU power used while AI algorithm is running?

 

Thanks

Suvo

 

 

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
May 29, 2024 8:35 AM UTC

Hi,

All the code is available in AutoDevKit Studio, just load the appropriate application.

 

Best Regards,

AutoDevKit Team

1 reply

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
May 29, 2024 8:35 AM UTC

Hi,

All the code is available in AutoDevKit Studio, just load the appropriate application.

 

Best Regards,

AutoDevKit Team