Skip to main content
Associate II
Feb 11, 2025 11:50 PM UTC
Solved

AEK-POW-BMS63EN showing incorrect cell voltages

Hey,

I am trying to build a battery pack with AEK-POW-BMS63EN BMS Slave Boards, AEK-MCU-C4MLIT1 as the Master Board, and an ISOSPI Translator. 

I have made a 4S Dummy Battery to check whether I could get the cell data on the serial bus from the Master Board. As suggested, I started working with the Example code titled 'SPC58EC-AEK_POW_BMS63EN_SOC_Est_SingleAccess_CHAIN application for discovery' but although the code got flashed onto the master board, I was still reading '0' values from the slave. 

Again, I tried the program titled 'SPC58EC - AEK_POW_BMS63EN_SOC_Estimation_Single application for discovery', since I realized that there was no ISOSPI Component added in the previous project. With this example project, I started getting some values but they seem incorrect. I am getting 5.8V on Cell 1 and 0V on the rest of the cells even when I checked the voltage on the test pins on the board between C0 and C1 is 3.8V. 

I am definitely doing something wrong here, I will take a look at the wiring again tomorrow. But, please help me out if anyone has faced this issue before. Thanks. 

PS: Should I try the example project titled 'SPC58EC - AEK_POW_BMSWTX_SOC_Est_SingleAccess_CHAIN application for discovery' as it supposedly has the latest driver code but it is for AEK_POW_BMSWTX Board right? Will it work for the AEK-POW-BMS63EN BMS Slave Boards?

 

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Feb 26, 2025 1:54 PM UTC

Hi,

There are constraints in connecting a battery pack with less than 14 cells:

- the minimum 4 cells should include the first two and the last two

- all the sensing and balancing signals should be connected or the voltage reading will not work

Please refer to the user manual

https://www.st.com/resource/en/user_manual/um3185-getting-started-with-autodevkit-battery-management-system-bms-evaluation-boards-stmicroelectronics.pdf 

Best Regards,

AutoDevKit Team

 

2 replies

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Feb 26, 2025 1:54 PM UTC

Hi,

There are constraints in connecting a battery pack with less than 14 cells:

- the minimum 4 cells should include the first two and the last two

- all the sensing and balancing signals should be connected or the voltage reading will not work

Please refer to the user manual

https://www.st.com/resource/en/user_manual/um3185-getting-started-with-autodevkit-battery-management-system-bms-evaluation-boards-stmicroelectronics.pdf 

Best Regards,

AutoDevKit Team

 

VipulsAuthor
Associate II
Feb 26, 2025 2:03 PM UTC

Thank you Max! 

I figured it out eventually. I was making a mistake with the Cell 0 connection. Thanks!