Skip to main content
Associate III
Nov 1, 2024 10:17 AM UTC
Solved

AEK-POW_BMS63EN cell balancing manually adjust

Dear community members,

 

There are multiple functions related to cell balancing in AEK-POW_BMS63EN_id. However, when I tested, none of them work. Here is my main code based on the "SPC58EC - AEK_POW_BMS63EN_SOC_Estimation_14Cells_GUI application for discovery" example. Could anyone experts give me documents about how to manually use cell balancing of this board? and explain detail how cell balancing of AEK-POW-BMS63EN works?

This is my code:

trishuynh_0-1730455880757.png

And this is the results: Cells balancing still turn on

trishuynh_1-1730455908832.png

 

This topic has been closed for replies.
ATROI
ATROIBest answer
ST Employee
Nov 27, 2024 2:39 PM UTC

Hi Trishuynh,

There was probably a misunderstanding in my first response to your question.
I will try to be more clear. The function AEK_POW_BMS63EN_Start_Mgn_exec() start a process that ciclically activate cell balancing.
This means that if you use this function with no changes, cell balancing is activated periodiacally.
If you want to change the behaviour of cell balancing, before to call in your main AEK_POW_BMS63EN_Start_Mgn_exec(), you should modify the function AEK_POW_BMS63EN_Balancing() according to your needs.  see image below.

 

ATROI_0-1732718269015.png

We suggest updating AutoDevKit, in order to use the new driver on BMS (BMS_CHAIN)
that has been released and to use the demo: SPC58EC - AEK_POW_BMS63EN_SOC_Est_SingleAccess_CHAIN application for discovery.

take into account that the old library is deprecated.

Thanks,

AutoDevKit Team

12 replies

ATROI
ST Employee
Nov 5, 2024 12:58 PM UTC

Hi Trishuynh,

 

In the function AEK_POW_BMS63EN_StartMgn_exec there is a set of functions that, based on the SOC, activates the cell balancing. Executing this function after StopCellBalancing, DisableCellBalancing ... overrides the expected behavior.

We suggest updating AutoDevKit, in order to use the new driver on BMS (BMS_CHAIN)
that has been released and to use the demo: SPC58EC - AEK_POW_BMS63EN_SOC_Est_SingleAccess_CHAIN application for discovery.

Regarding your request for documentation in the folder comments -> aek_pow_bms63chain_component_rla -> doc
you will find the file in which the functionality of each function is described.

Finally, below a list of some function that you should use to achieve your scope:

//Set Balancing Mode of Node of BMS Chain.

- AEK_POW_BMS63CHAIN_node_setBalMode


//Enable Balancing Cell of Node of BMS Chain.
- AEK_POW_BMS63CHAIN_node_enableBalCell


//Disable Balancing Cell of Node of BMS Chain
- AEK_POW_BMS63CHAIN_node_disableBalCell


//Set Balancing Start of Node of BMS Chain.
- AEK_POW_BMS63CHAIN_node_setStartBal


//Set Balancing Stop of Node of BMS Chain.
- AEK_POW_BMS63CHAIN_node_setStopBa

Thanks,

AutoDevKit Team.

trishuynhAuthor
Associate III
Nov 22, 2024 9:47 AM UTC

Dear ATROI,

 

I followed your instruction that use new driver on BMS (BMS_CHAIN). When I run the demo SPC58EC - AEK_POW_BMS63EN_SOC_Est_SingleAccess_CHAIN application for discovery, everything works perfectly. Then, In the function AEK_POW_BMS63CHAIN_app_step, I uncomment all the code of Balancing and replace them with 2 lines of code:

AEK_POW_BMS63CHAIN_node_setBalMode(AEK_POW_BMS63CHAIN_CHAIN0, AEK_POW_BMS63CHAIN_NODE_DEV1, AEK_POW_BMS63CHAIN_BAL_MANUAL);
AEK_POW_BMS63CHAIN_node_setStopBal(AEK_POW_BMS63CHAIN_CHAIN0, AEK_POW_BMS63CHAIN_NODE_DEV1);

 

However, when I run the program, the balancing is still on. I have several questions could you and experts help me:

 

1. How and where to use the balancing functions in the demo provided.

2. When enable the balancing, can I have fully permission to change the balancing value of each cells to 0 or 1?. Or these values are automatically turned on by the system?

 

I also attached the picture of the code and the output for your references.

Thank you for your attention to this matter. I appreciate your assistance in clarifying this detail.

Best regards,

Trishuynh.

trishuynh_0-1732268547110.png

trishuynh_1-1732268555046.png

 

 

 

ST Employee
Nov 22, 2024 4:25 PM UTC

Hello,

It might be easier to help you if you shared a snapshot of the following data structures:

AEK_POW_BMS63CHAIN_fastMeas_t

 AEK_POW_BMS63CHAIN_fastDiag_t

Please, could you attach a txt file with structure field data?