Skip to main content
Associate II
Feb 24, 2024 6:23 PM UTC
Solved

AEK-POW-BMS63EN as a Master Board in the daisy chain

Hi,

I would like to check if STM AEK-POW-BMS63EN board can be used as a first board in the daisy chain with the setup where we have external MCU (for example STMF103RB) and AEK-COM-ISOSPI1?

In the datasheet you describe difference between 'Master' and 'Slave' in the following way:

MaraLo_0-1708798358615.png

and all your AEK-POW-BMS63EN comes with SPEIN pin pull-down via R20:

 

MaraLo_2-1708798811017.png

Can you please clarify if the usage of AEK-POW-BMS63EN in the single BMS setup with external MCU is even possible?

BR,

MaraLo

This topic has been closed for replies.
Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Feb 24, 2024 7:52 PM UTC

hi,

Yes, for a single node you can use STM32 SPI to AEK-COM-ISOSPI1 and connect the AEK-COM-ISOSPI1 to the AEK-POW-BMS63EN.

Be careful that endianess of STM32 and SPC5 is different (big endian).

Best Regards,

AutoDevKit Team

 

1 reply

Max VIZZINI
Max VIZZINIBest answer
ST Technical Moderator
Feb 24, 2024 7:52 PM UTC

hi,

Yes, for a single node you can use STM32 SPI to AEK-COM-ISOSPI1 and connect the AEK-COM-ISOSPI1 to the AEK-POW-BMS63EN.

Be careful that endianess of STM32 and SPC5 is different (big endian).

Best Regards,

AutoDevKit Team