Skip to main content
kim sunho
Visitor II
Jul 18, 2017 3:11 PM UTC
Question

Why the TDA7491LP / mute input is low

Posted on July 18, 2017 at 17:11

#Help.!!! The TDA7491LP mute pin is the input port. I connected the 3.3V pullup resistor 33K resistor to the power supply, and the mute pin keeps the state of LOW state .... What is the cause? So there is no sound. .   Keep mute ...?

    This topic has been closed for replies.