Skip to main content
nmagniez
Visitor II
January 16, 2014
Question

What is the STSmartVoice Demo Kit?

Posted on January 16, 2014 at 17:19

What is the STSmartVoice Demo Kit?

    This topic has been closed for replies.

    3 replies

    Marco VENERI
    ST Employee
    January 17, 2014
    Posted on January 17, 2014 at 16:47

    The

    http://www.st.com/web/en/catalog/tools/FM116/SC1028/PF255176

    is an evaluation board specifically designed to interface with ST Digital

    http://www.st.com/memsmics

    . The kit is based on a digital audio processor, STA321MP, able to interconnect up to 6 digital PDM microphones, convert signal from PDM to PCM and apply pre-processing filtering and equalization before feeding its output interface, either I2S or PWM/HP.

    Together with the

    http://www.st.com/web/en/catalog/tools/FM116/SC1028/PF258331

    interface the kit can be used to conveniently upstream the microphone signals via USB and analyze acquired data with

    http://www.st.com/web/en/catalog/tools/FM147/SC1857/PF258785

    tool, in real-time.

    davidg.shaw9
    Associate
    July 3, 2014
    Posted on July 03, 2014 at 17:41

    How many different mic channels can I record simultaneously with the complete STSmartVoice kit that includes the STAudioHub?

    What recording software will I need for Windows 7?

    I have Audacity, but I cannot see more than two channels (stereo).

    Thanks for any help.

    David Shaw

    Marco VENERI
    ST Employee
    July 18, 2014
    Posted on July 18, 2014 at 14:57

    Hi David,

    The STSmartVoice kit upstream the audio via the AudioHub kit which only allow for a stero recording (ie. 2 channels).

    If STAudioHub is used with APW, with or without the SmartVoice kit, then the recording option is offered directly by APW itself and it's not possible to use external sw.

    Should you prefer to use your own audio recording software - such as Audacity - you need to run STAudioHub in standalone mode so that it will enumerate as a standard audio acquisition USB card.

    Also - though not relevant to STSmartVoice/AudioHub - note that Audacity is not supporting more than 2 channels on Win7 due to some licensing problem with the ASIO drivers. You'll need to have a custom build of the sw - including ASIO - in order to enable multi-channel audio.

    Regards,

       Marco