Skip to main content
Junfeng Liao
Associate
January 24, 2017
Question

TDA7498E

Posted on January 24, 2017 at 10:22

As we know, TDA7498E is designed for Audio amplifier application.  But we are interested in using it for DC amplifier application.

In our application, an inductance coil is connected to amplifier output. This load is up to 24VDC / 3A max, so Class D amplifier is idea for it.

But the operating frequency range is from 0Hz-100Hz, which is different with Audio application. Can we just remove the DC-block capacitor from the input circuit, and use TDA7498E in this DC amplifier application?

#tda7498e
This topic has been closed for replies.

2 replies

Junfeng Liao
Associate
January 29, 2017
Posted on January 29, 2017 at 12:19

Why there is no reply since 5 days ago? Is this forum alive?

Tesla DeLorean
Guru
January 29, 2017
Posted on January 29, 2017 at 17:01

Areas of the forum are alive, but are always dependent on participation.

Review with other engineers at you own company, and perhaps prototype/experiment.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..