Skip to main content
cperuj23
Associate II
July 31, 2015
Question

TDA7384A: Sink size, power dissipation and load

Posted on July 31, 2015 at 18:58

Hello,

I'm modifying a device that no works very well. This device includes one amplifier TDA7384A, and in the old design I found several mistakes or parameters that haven't calculated. I saw the datasheet and i didn't know how can i calculate some parameters with the information in the datasheet:

- If the power supply is 12V, How can I calculate the power dissipated?

- Apart of power dissipated, for calculate the size of the sink, Is not necessary to know the Rcd of the Flexiwatt25? 

- The device have a load resistance of 8 Ohm and the TDA7384A is designed for 4 Ohm. Can a 8 Ohm load modify the response of the amplifier or only decrease the power?

Thanks

Carlos
This topic has been closed for replies.

8 replies

Nickname1623_O
Visitor II
August 3, 2015
Posted on August 03, 2015 at 05:05

Hi Carlos ,

the power dissipation could be calculated with below formula , TDA7384 is single supply BTL output configuration power amplifier , then the power dissipation is :Pd= 2*(VCC^2)/((3.14^2)*RL).

to calculate the heatsink size , you need to check the thermal impedance between heatsink and ambient , then you can consider that the power dissipation is as current , thermal impedance is as resistor , then ambient temperature , IC case temperature and IC junction temperature as voltage potential level. when the target temperature had been set , you can choose suitable heatsink. the Rth of package is 1C/W , means that the temperature difference between junction and case will be 10C , when dissipation power is 10W .

the 8 ohm load will just decrease the output power .

Thanks ,

YT

cperuj23
cperuj23Author
Associate II
August 3, 2015
Posted on August 03, 2015 at 12:16

Hello YT!

Thanks for your quick response! It has been very useful

cperuj23
cperuj23Author
Associate II
August 7, 2015
Posted on August 07, 2015 at 11:33

Hello,

I have another doubt of TDA7384A. For calculate the power supply:

First, I have looked the Figure 8 and for a power supply of 12V I have 18W of power output (THD 10%). Secondly, I have looked the Figure 13 and the total power dissipation (for the four channels in 13.2V) is 35W for 18W of power output. Is that means that I need a power supply of (PS = (18*4) + 35) 107W (approx.)? or Are there another method to calculate the power supply? (PS = Io^2*Rload)

Sorry for all of questions, the University teachs a lot of theoretical aspects but very little practical experience.

Thanks,

Carlos

Nickname1623_O
Visitor II
August 25, 2015
Posted on August 25, 2015 at 09:34

Hi Carlos ,

Yes, in theroy  you need 107W power supply to  provide enough power to amplifier for 4 channels 18W continous output power .

due to music signal is dynamic signal and the average power is around 1/3 continous output power ,or you can consider to delivery full power continously in stereo channel , so you can use a 70W (12V @ 5A ) supply to reach similar speaker output loudness, of cource , you need to put big VCC bypass capacitor close to power amplifier IC to provide high transient current.

Thanks,

YT

vinod
Visitor II
September 28, 2015
Posted on September 28, 2015 at 09:51

Hi,

 If we use this formula Pd= 2*(VCC^2)/((3.14^2)*RL) 

for VCC=13.2V and RL=4 ohm than Pd=8.82W and for 4 channel it will be 4X8.82W=35.30W.

But from datasheet fig 8 at 13.2V Pout will be 22Watt@10% THD and from Fig 13 power dissipation at 22W will 30Watt.

There is a ~5Watt difference between formula and datasheet. Please tell which Pd should be used?

regards

Vinod

Nickname1623_O
Visitor II
October 10, 2015
Posted on October 10, 2015 at 03:22

hi Sharma,

in fact ,there are no conflict between those data, since the max dissipation power is at 1/3 output power , and with max output power , the efficiency of ampilifer is best, then power dissipation had been reduced .

thanks

YT

scott23
Visitor II
May 9, 2016
Posted on May 09, 2016 at 09:02

scott23
Visitor II
May 14, 2016
Posted on May 14, 2016 at 10:11