Skip to main content
Visitor II
March 22, 2024
Question

TDA7292 with Single Supply

Hi, I made a circuit for the TDA7292 with a simple power supply as shown in the brochure. The standby and off functions work well, but the low tones become distorted when I increase the volume more. The circuit works with 12VDC. Is it because more DC voltage is needed? or do you have to make an additional modification to the output?

Thanks in advance.

single_tda7292.png

This topic has been closed for replies.

1 reply

AScha.3
Super User
March 22, 2024

Hi,

at 12V (car voltage) you can expect about 4W max.

So no "ear killer" volume possible. :)

see:

AScha3_0-1711118500719.png

So for 40W you need +/-26VDC , or 50V total.

If you feel a post has answered your question, please click on " Best Answer ".