Skip to main content
Associate
July 11, 2024
Question

tda 7560 ic not working problem

I bought this chip and pcb circuit from the internet, then when I plugged all the components into the pc and powered it up, I couldn't get any sound. When I powered up the circuit, it got hot inside, but only a low sound came from one speaker pin, but it didn't reflect the sound I gave to the speaker in any way. Also, this heating situation happens when there is no st-by short circuit. When I checked it with the short circuit-diode stage of the multimeter, when I filled the capacitor a little and touched the legs of the channel with low sound to GND, it showed a short circuit and stopped after a while, so I think there is a short circuit between the power input and the channel with low sound, and when I touched its negative end to GND and the other end to the output of the channels, I see 600 in the outputs without low sound, while I see 70 and 100 in the channel with hiss. These are what I found for now, thank you very much if you can help. Also, I want to ask something, do we need to short-circuit the st-by and mute pins and leave them or do we need to keep them in the short circuit position when we use them?

This topic has been closed for replies.

6 replies

Peter BENSCH
ST Technical Moderator
July 12, 2024

Welcome @FicoresS, to the community!

  • Do you have any knowledge of electronics in general and audio amplifiers in particular?
  • What kind of board did you buy and where?
  • Have you looked at the schematics of the board?
  • Does the board have a heat sink?
  • What kind of power supply do you have for the board?
  • What kind of loads (speakers) with what parameters have you connected?
  • Are these speakers in an enclosure?
  • What audio source with what voltage is connected to the inputs of the amp?

These are just initial questions, as you have provided practically zero useful information.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
FicoresSAuthor
Associate
July 13, 2024

I have some knowledge in general.

I took the PCB from the layout in the datasheet and arranged it myself and printed it.

Yes, I looked at the schematic

Yes, there is a heatsink

I used a 3s Li-ion battery pack

I connected a 4 ohm speaker just to test it

The speakers are bare

I connected 11.8V as power and it drops to 11.5 volts when the circuit is active.
I used both a computer and a phone as audio input

There is something I didn't mention extra, while making the connections in the circuit, I connected in1 and in2 directly in parallel and connected a capacitor to the end, then I gave an audio input from the other end of those capacitors.

AScha.3
Super User
July 13, 2024

Show a pic from your amp construction .

And a link, what you bought .

If you feel a post has answered your question, please click on " Best Answer ".