Skip to main content
MRUEF.1
Visitor II
May 16, 2023
Question

STP16NF06 vs IRF520

IRF520 type MOSFETs are starting to be phased out and so in all review, STP16NF06 should be a stable cross reference from what I have read, would anyone know perhaps is there a better cross for an IRF520 than the ST STP16NF06? i have ask OnSemi and their idea on this question is not much help as they point to MOSFETs that actually lower in current and PD

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    May 16, 2023

    Welcome, @MRUEF.1​, to the community!

    You are obviously using the IRF560 in the TO-220 package variant, right?

    I know this MOSFET with a maximum drain voltage of 100V, Rdson max 0.2ohms and a continuous current of max 6.8A at 100°C.

    The STP16NF06 you have chosen can only handle 60V, but more current with a smaller Rdson.

    For max 100V I rather recommend the STP24NF10 with 100V, max 0.06ohms and 18A at 100°C. There are many more suitable types with considerably better parameters, but a more precise selection only makes sense if you know your application and exact requirements (frequency, driving, etc).

    Hope that helps?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.