Skip to main content
JSun.5
Visitor II
March 3, 2023
Question

STA350BW功放的频�?�?�以达到40kHz�?�? Is it possible to have up to 40kHz frequency response on STA350BW amplifier?

  • March 3, 2023
  • 2 replies
  • 864 views

如果通过调节STA350BW输出的LC滤波器,�?�以将频�?延伸至40kHz�?�?输入I2S采样率为192kHz。

Is it possible to set the frequency response of STA350BW to up to 40kHz by having a higher cut-off frequency LC filter? The I2S input frequency is set to 192kHz.

    This topic has been closed for replies.

    2 replies

    Peter BENSCH
    ST Technical Moderator
    March 3, 2023

    Welcome, @JSun.5​, to the community!

    We will check the question internally and then get back to you, for which we ask for a little patience.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    PZHAN.1
    ST Employee
    March 10, 2023

    Hello JSun.5, warmly welcome to join our community for the frequency response extending to 40KHz discussion. allow me reply your question: the answer is yes, our STA350BW can ​set up to 40KHz by LPF of LC main network, the curves here I attached the some simulation of different Rloads such as 4ohm and 8ohm conditions.0693W00000aIdElQAK.pngkindly let's know if there is anything unclear about ST Audio products.

    Thank you for your great cooperation!

    Best Regards,

    Peter ZHANG