Skip to main content
Visitor II
November 13, 2023
Solved

Question about LMV321LICT

Dear Sirs!

 

I use in my design LMV321LICT manufactured by STMicroelectronics. And I faced very strange behavior.

LMV321LICT powered by +3V in mode of buffer or non inverting amplifier.

When for example there is +1.5V DC in plus input and gain 2, I see about +3V in output (no load).. It really work as rail to rail amplifier as expected.

But when there is +3V DC in plus input and gain 1, I see about +2.5 V on output (no load) but I expected to see +3V.

I have not found in datasheet any limitations about input voltage.

Can you please explain?

Is it a correct behavior for this amplifier or something wrong in my board?

Best regards

Michael

 

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
November 13, 2023

is as in ds :  max. input Vcc-1V ; so at 3V vcc max. 2V at input. 

AScha3_0-1699897350813.png

+ if you want input range 0..vcc , need R2R input and output opamp !

If you feel a post has answered your question, please click on " Best Answer ".

2 replies

AScha.3
AScha.3Best answer
Super User
November 13, 2023

is as in ds :  max. input Vcc-1V ; so at 3V vcc max. 2V at input. 

AScha3_0-1699897350813.png

+ if you want input range 0..vcc , need R2R input and output opamp !

If you feel a post has answered your question, please click on " Best Answer ".
Visitor II
November 13, 2023

You can find the information mentioned by the above answerer in paragraph 4.2 in the datasheet.

https://www.mouser.com/datasheet/2/389/lmv321l-1849682.pdf