Skip to main content
Associate II
April 22, 2024
Question

LMV321ILT 3.3V operational compatibility

Hi,

@Peter BENSCH 

In the datasheet of ST LMV321ILT op-amp, it is stated that minimum voltage supply span is 2.7V and maximum supply span is 6V. Can you suggest whether LMV321ILT can be used with 3.3V or an alternate that is both pin to pin and 3.3V compatible? Also, the VOH VOL characteristics are defined for VCC=5V and VCC= 2.7 V. Could you also provide VOH VOL levels when VCC =3.3V if the op-amp is compatible with supply of 3.3V?

 

Regards,
Sreejith

This topic has been closed for replies.

2 replies

LCE
Principal III
April 23, 2024

Read the datasheet!

> Operating range from VCC = 2.7 to 6 V

Yes, it works with 3.3V.

 

> Also, the VOH VOL characteristics are defined for VCC=5V and VCC= 2.7 V. Could you also provide VOH VOL levels when VCC =3.3V if the op-amp is compatible with supply of 3.3V?

An operational amplifier is (usually) a purely analog circuit, so you can basically interpolate its 3.3V behavior from the values given at 2.7V and 5V.

In case of doubt, take the worst (min / max) values of both.

ST Employee
April 24, 2024

Hi All,

 

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

 

Regards,
Jake

ST Support