Skip to main content
JSimo.19
Associate
February 8, 2019
Question

LM2901 with one input outside the input common mode range

In the data sheet for TSX339 it says in chapter 6.1:

 "The output state is guaranteed as long as one input remains within the common mode

input voltage range (defined in the operating conditions table), and the other input remains

between -0.3 V and 16 V (meaning that one input can be driven above VCC+)."

Is the same true for LM2901, i.e. one input within the common mode input voltage range and the other input between -0.3 V and 36 V?

    This topic has been closed for replies.

    6 replies

    MikeDB
    Senior II
    February 19, 2019

    I believe so yes.

    JSimo.19
    JSimo.19Author
    Associate
    February 20, 2019

    Thanks for answering but I would not select this circuit though until someone from ST says that this is really the case.

    MikeDB
    Senior II
    February 20, 2019

    Select which - the TSX339 or the LM2901 ? The LM2901 is a generic part from numerous manufacturers and it was this part your question seemed to be addressing.

    JSimo.19
    JSimo.19Author
    Associate
    February 20, 2019

    The circuit I would like to use is the LM2901 from ST if I can trust it only needs one of the input pins to be inside the specified common mode range and still have the right "result" on the output pin

    MikeDB
    Senior II
    February 20, 2019

    Well as it's a generic part I doubt ST even designed it - they probably just copied the original and that was forty years ago so no-one will give any guarantees. Why not play safe and use resistive dividers on both pins to bring the voltages well within the rail voltages ?

    JSimo.19
    JSimo.19Author
    Associate
    February 20, 2019

    I see I had missed that this is already guaranteed in note 4 below table 3.