Skip to main content
esisw.1
Associate
March 2, 2022
Solved

If i buy BD 140 only- is it same with BD 140 -16 or BD 140- 10?

..

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    March 2, 2022

    Welcome, @esisw.1​, to the community!

    The pnp bipolar transistor BD140 will be supplied in three groups of the parameter hfe (see datasheet, page 4):

    • BD140: 40...250
    • BD140-10: 63...160
    • BD140-16: 100...250

    Of course, it always depends on the circuit, but most of the time you can replace a BD140 with a BD140-10 or BD140-16, but not necessarily vice versa.

    If you want to be sure that the circuit works safely with the BD140 instead of the BD140-10 or BD140-16, you have to measure the value of hfe of the BD140 and make sure that you are in the appropriate group with it.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    2 replies

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    March 2, 2022

    Welcome, @esisw.1​, to the community!

    The pnp bipolar transistor BD140 will be supplied in three groups of the parameter hfe (see datasheet, page 4):

    • BD140: 40...250
    • BD140-10: 63...160
    • BD140-16: 100...250

    Of course, it always depends on the circuit, but most of the time you can replace a BD140 with a BD140-10 or BD140-16, but not necessarily vice versa.

    If you want to be sure that the circuit works safely with the BD140 instead of the BD140-10 or BD140-16, you have to measure the value of hfe of the BD140 and make sure that you are in the appropriate group with it.

    Does it answer your question?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    esisw.1
    esisw.1Author
    Associate
    March 9, 2022
    Dear Mr Peter
    Thank you for your information.
    This answered my question.
    Best regards
    Edie S