Skip to main content
MDarw.1
Associate
November 19, 2021
Question

I'm trying to work with STAPI003 audio amplifier, in the datasheet it says that it 4 x 52 W/4 Ω max, but i am not able to get more than 32 watt at 4 ohm. How can i achieve above 32 watt, is it possible to bridge the output?

..

    This topic has been closed for replies.

    4 replies

    MM..1
    Super User
    November 20, 2021
    • 4 x 52 W/4 Ω max.
    • 4 x 30 W/4 Ω @ 14.4 V, 1 kHz, 10 %

    How is your Vcc ? For more power you need more Vcc...

    MDarw.1
    MDarw.1Author
    Associate
    November 20, 2021

    Hello,

    My Vcc is accurate 14.4V DC with 30amp available current. The supply voltage is not dropping when try to increase the sine wave source input, when the output goes above 32 watt it start clipping. So the maximum stable output i could reach at 4 ohm was 32 watt. Is there any trick for this IC to increase the output level?

    MM..1
    Super User
    November 20, 2021

    I can only repeat trick is more Vcc see docu for max.

    MDarw.1
    MDarw.1Author
    Associate
    November 20, 2021

    How about bridging the outputs, can this IC support this feature?