Skip to main content
SChun.4
Visitor II
Apr 24, 2019 2:45 PM UTC
Question

How to configure a STEVAL-IME012V1 with the STSW-IME011 on Windows 10 OS?

How are you?

I would like to test an ultrasound pulser IC evaluation board (STEVAL-IME012V1) on Windows 10 PC. I installed a test software (STSW-IME011) to configure waveforms (frequency and number of pulses) for the evaluation board. However, I have not connected the evaluation board to the Windows 10 PC. The PC has not shown a suitable COM port (USB- 5 pin connection) yet. Would you please show me how to find the evaluation board on the Windows 10 PC?

Actually, I connected only with the 5-pin USB port to the PC. Should I connect power lines to the evaluation board?

Thank your for your help.

This topic has been closed for replies.