Skip to main content
전형진.1
Associate
April 11, 2023
Solved

How can I use differential audio input at TDA7292?

Hi, I'm trying to design hifi amplifier using TDA7292 refering its datasheet.

I read the datasheet of TDA7292, and I have some following questions :

​

  1. How can I use differential audio input at TDA7292? Is it okay to connect amplifier's IN1- and IN2- pin to differential audio source's L- and R- pin instead of connecting those amp pins to GND?
  2. With a single supply circuit, is it okay to supply single +48V 2A power to TDA7292? In TDA7292's electrical absolute maximum ratings, it the maximum DC supply voltage of TDA7292 is +-35V. But what I'm trying to design is single supply circuit. I wonder if it would be overloaded.
  3. Is there are any disadvantage using 'For Single supply' circuit instead of using 'For Dual rail supply' circuit?
  4. I found what I assume to be an error in the Figure22 diagram on page 17 in the datasheet. Pin 2 of the TDA7292 is OUT1 and pin 10 is IN1-, but in Figure 22 they are reversed. It seems to me that this is an error, am I right?

​

I'm newbie in circuit design, so please understand me if there are any sound like dumb​ question.

Thank you! :grinning_face:

This topic has been closed for replies.
MasterT
MasterTBest answer
Lead II
January 18, 2024

How can I use differential audio input at TDA7292? Is it okay to connect amplifier's IN1- and IN2- pin to differential audio source's L- and R- pin instead of connecting those amp pins to GND?

 L & R is not differential outputs, but single ended left & right.

With a single supply circuit, is it okay to supply single +48V 2A power to TDA7292? In TDA7292's electrical absolute maximum ratings, it the maximum DC supply voltage of TDA7292 is +-35V. But what I'm trying to design is single supply circuit. I wonder if it would be overloaded.

 You can use single power, +70V

Is there are any disadvantage using 'For Single supply' circuit instead of using 'For Dual rail supply' circuit?

 Yes, there is disadvantage in using electrolitic capacitors, find a DS for TDA2030 and study amp with single power.

I found what I assume to be an error in the Figure22 diagram on page 17 in the datasheet. Pin 2 of the TDA7292 is OUT1 and pin 10 is IN1-, but in Figure 22 they are reversed. It seems to me that this is an error, am I right?

Agree, typo error. Use pin desciption with figure 2

4 replies

전형진.1
Associate
April 11, 2023
Visitor II
January 18, 2024

Hi,

In datasheet there is no Bridge Circuit and recommended supply details. If I want to convert single output capable to drive 80W max.

 

Can Any one provide the Bridge Circuit Schematic and recommended supply for bridge circuit.

AScha.3
Super User
January 18, 2024

Hi,

try:

 

AScha3_1-1705567767874.png

 

If you feel a post has answered your question, please click on " Best Answer ".
MasterT
MasterTBest answer
Lead II
January 18, 2024

How can I use differential audio input at TDA7292? Is it okay to connect amplifier's IN1- and IN2- pin to differential audio source's L- and R- pin instead of connecting those amp pins to GND?

 L & R is not differential outputs, but single ended left & right.

With a single supply circuit, is it okay to supply single +48V 2A power to TDA7292? In TDA7292's electrical absolute maximum ratings, it the maximum DC supply voltage of TDA7292 is +-35V. But what I'm trying to design is single supply circuit. I wonder if it would be overloaded.

 You can use single power, +70V

Is there are any disadvantage using 'For Single supply' circuit instead of using 'For Dual rail supply' circuit?

 Yes, there is disadvantage in using electrolitic capacitors, find a DS for TDA2030 and study amp with single power.

I found what I assume to be an error in the Figure22 diagram on page 17 in the datasheet. Pin 2 of the TDA7292 is OUT1 and pin 10 is IN1-, but in Figure 22 they are reversed. It seems to me that this is an error, am I right?

Agree, typo error. Use pin desciption with figure 2