Skip to main content
GScha.1
Associate
January 13, 2022
Question

Hello, I would like to know the Power Dissipation of USBLC6-2P6 (SOT666 package). I did not find any info in the datasheet. Thanks you, G.Schaeffer

..

    This topic has been closed for replies.

    2 replies

    Peter BENSCH
    ST Technical Moderator
    January 13, 2022

    Welcome, @GScha.1​, to the community!

    The power dissipation is actually only important for TVS diodes because their test pulses last considerably longer. With ESD diodes, however, this is not important because ESD pulses are in the nanosecond range

    Is there a specific reason you want the power dissipation specified?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    GScha.1
    GScha.1Author
    Associate
    January 13, 2022

    Thanks for your answer,

    I have to certify a product for ATEX (explosive atmospheres) : Thermal ignition consideration. / Directive 2014/34/EU

    The temperature of a mounted component must not exceed 270°C (in case of an short-circuit for example). That is why they are looking for the power dissipation and the Rth.

    Best regards,