Skip to main content
Associate II
November 28, 2023
Question

Driving 2 headset in parallel with ts482idt audio amplifier

  • November 28, 2023
  • 3 replies
  • 1761 views

Hi, 

I'm wondering if it is okay to connect 2 16ohm headsets in parallel to the ts482idt stereo amplifier. This would mean that the output load is now 8ohms but the datasheet only mentions 16 and 32 ohm loads. What if any issues would I encounter in this configuration?

 

Thanks, 

 

This topic has been closed for replies.

3 replies

AScha.3
Super User
November 28, 2023

AScha3_0-1701205253223.png

at 5V:

AScha3_0-1701205475502.png

so about 80 mW in 8 ohms. you should put 8 or 10 ohms at the output, so not producing too low impedance to the amp.

why connect 2 x 16 ohm par. ?  why not connect in series ... ?

If you feel a post has answered your question, please click on " Best Answer ".
Kenny03Author
Associate II
November 28, 2023

since we're using a standard stereo headset here. the left and right speakers have the return lines both connected to one analog ground so it would not be possible to do a series connection. So the concern with the too low impedance is that it might pull more current than the max output spec? Our audio output is very low power (50mV and 6mA rms), so it should be okay right?

AScha.3
Super User
November 29, 2023

okay; if you want keep the spec , add a 10 ohm at the output, so the amp gets : 8 + 10 = 18 ohm load.

If you feel a post has answered your question, please click on " Best Answer ".