Skip to main content
Md Mubdiul Hasan
Associate III
September 26, 2019
Question

Does ST provide ClassD amplifier application for transformer ?

Hi,

Hope this post find you well.

My intention is to make an 3-phase power calibrator !

Similar to this link, https://us.flukecal.com/products/ele...wer-calibrator

0690X000009jHLvQAM.jpg

My current AMP design might be class AB type.

I am not worried to much about PWM generation ruther I am thinking how can I move class AB to Class D amplification.

A lot of the design effort relates to maintaining linearity and avoiding crossover distortion.

In this case, 2 amplifiers( current, voltage) output will feed to CT and PT!

Lets consider transformer load .

REQUIRMENTS :

1. The amp input should be plus and minus 7volt AC, 45-65Hz( 1 Hz has been converted to 1024)

2. Amp operating voltage should be more or less 24v.

3. 2 channel signal (not sure PWM) should be use , one for current, one for voltage.

4.Can run current transformer(input 16.5 V/1.5 A) and potential Transformer (input15v/2A). PT output may be 15VAC.

5. If possible both voltage and current amplification is required in one IC.

6. Both positive and negative half signal should be amplify

    This topic has been closed for replies.