Skip to main content
gene-zhen
Visitor II
November 28, 2014
Question

Difference between LM224 and LM224A

Posted on November 28, 2014 at 09:04

Hi,

Is there tmeperature drift difference between the two types? Or is there any other difference between the two type,please?

Thanks!

This topic has been closed for replies.

1 reply

Nickname560_O
Visitor II
November 28, 2014
Posted on November 28, 2014 at 11:38

Hi wang.zhen.003,

For most of ST operational amplifier product the A label define a product with a better Vio.

You don’t have any difference one the DVio/DT = 7µV/°C in typical value or 30µV/°C for max value in the both cases.

If you compare the max Vio value between LM224 and LM224A you can see a difference of 2mV.

Ambient:5mV -> 3mV(A version)

Temperature:

7mV -> 5mV(A version)

Regards

Florian