Skip to main content
jmoore
Visitor II
September 30, 2013
Question

Configuration, set-up or help files for APWorkbench with MEMS

Posted on September 30, 2013 at 15:53

Are there any example apc files for the MEMS microphone demonstrator? as indicated in the application note: AP4146, For example basic directional microphone set-up. There seems to be no Help available or very little supportive documentation for these boards.

    This topic has been closed for replies.

    1 reply

    Marco VENERI
    ST Employee
    October 1, 2013
    Posted on October 01, 2013 at 09:23

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00061574.pdf

    includes all relevant information about the 

    http://www.st.com/web/en/catalog/tools/PF255176

    board usage. Additional material is also available for each specific board which could operate with it, such as

    http://www.st.com/memsmics

    or the

    http://www.st.com/web/en/catalog/tools/PF258331

    interface.

    Configuration files (.apc) can be either created by the user or provided by ST upon specific request - contact an ST representative in case of need.