Skip to main content
andrew sauter
Associate II
June 9, 2017
Question

Can under-powering an OpAmp Damage it (TSV358AIDT)

Posted on June 09, 2017 at 05:47

We are seeing some of our opamps failing, outputting the VCC rail regardless of input!

The input signal is a BLDC fan current sense resistor and cell a is a non-inverting gain of 3x.

Our sleep circuit was implemented incorrectly, during sleep Vcc is actually 1.5V instead of 0V, can this damage this part (note: other pins should be at 0V until 3.3V is applied when woken)?

    This topic has been closed for replies.