Skip to main content
Ashar.2
Visitor II
June 9, 2022
Question

can i make stereo speaker for computer using TDA7269A ?

my old tea2025b speaker stopped working ,can i use this ic to make new stereo speakers or there is another better ic for making speakers ?

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
June 9, 2022

Welcome, @Ashar.2​, to the community!

It depends on what you mean by "better", as well as what exactly you want the amplifier to do. The TEA2025B was a stereo AB amplifier with a single supply that could be operated with voltages between 3...12V, but depending on the voltage it only delivered 0.1W to just under 3W output power.

The TDA7269A, on the other hand, is actually designed for split supply, i.e. positive and negative supply voltage between ±5...±20V. However, it can also be operated with single supply between 10...40V.

Now it depends on which supply voltage you have available and which load impedances are to be connected (4 ohms, 8 ohms, etc).

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.