Skip to main content
Associate
November 21, 2023
Solved

Application Note AN4835, High-side current sensing for applications using high common-mode voltage

In your application note, AN4835, you are using resistors R2 and R3. Please can you explain their purpose?

My circuit uses the TSZ121 precision op-amp in the classical method without R2 and R3 and it works equally well. 

Thank you very much for any insight you can provide.

Best regards, TK1

 

TK1_2-1700587777822.png

 

 

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
November 27, 2023

..just guessing:

- R2 sets some current limit (about 1mA) through bsp220, in case of a short/high current, to save the adc input

- R2 + R3 giving some added current gain, to get 3,3 V output with standard resistor values (otherwise 100A -> 3,03 V out)  -- not important, i think :)

If you feel a post has answered your question, please click on " Best Answer ".

5 replies

LCE
Principal III
November 23, 2023

Your picture does not show the important part that makes this work:

The zener diode and the resistor which create the supply reference voltage Vcc_L, which is Vcc_L = Vcc_H - Vzener.

So in this example the first opamp is actually supplied with 150 V and ~145 V.
Basically, R2 sets the gain, R3 allows and controls the output current through the MOSFET.

TK1Author
Associate
November 23, 2023

Thank you very much for your explanation. The Zener concept in HV supplies is an old one and well known.

The important part to me was to understand, the use of additional resistors that reduce accuracy, yet have no obvious benefit. Again, thanks for your fast help. Kind regards, Tom

LCE
Principal III
November 27, 2023

Okay, then you probably know more about that stuff than I do... :D

AScha.3
AScha.3Best answer
Super User
November 27, 2023

..just guessing:

- R2 sets some current limit (about 1mA) through bsp220, in case of a short/high current, to save the adc input

- R2 + R3 giving some added current gain, to get 3,3 V output with standard resistor values (otherwise 100A -> 3,03 V out)  -- not important, i think :)

If you feel a post has answered your question, please click on " Best Answer ".
TK1Author
Associate
November 28, 2023

This makes total sense. Why didn't I think of that?

Thank you very much for the quick and easy explanation. TK