Skip to main content
arivel1
Associate
May 28, 2021
Question

alarm and sound

Hello.

I would like to do the following but since I don't have the necessary skills I ask you. If possible, I prefer to control everything with the keys.

I make a list of the functions that I would like to implement:

ALARM SECTION

- wake up in the morning with a piece of music chosen at random from a list of music files in memory (each time a different music file is chosen. I had thought of a clock radio but I think it is better this way).

- daily or weekly alarm programming (i.e. the right to choose on which days the alarm should sound).

- automatic update of summer time - winter time

- buffer battery in case of power blackout (in this case I think the alarm with buzzer is better to consume little energy and not risk resetting the buffer battery)

- alarm disabling

AUDIO SECTION

- audio player with output that goes to the external I2s DAC.

four keys for playback, but I specify that each key corresponds to a single e

SINGLE music file. so in all 4 music files, of course they are different from each other.

- each key has the infinite loop function (when the song ends it restarts automatically).

- when the alarm time comes, the previous audio playback must be deactivated to allow the alarm to be activated.

- shutdown button.

I have never programmed and in general I have no programming knowledge but I know the principles of electronics.

to get the audio section I thought of using the ADkey mode as it is adopted by some play Mp3 / wav boards that are on the market. however I don't know if it can also be done with STM board.

if this were possible, I would only have the programming for the alarm clock section.

I have already found a piece of the program, the one for daylight saving time

https://www.instructables.com/The-Arduino-and-Daylight-Saving-Time-Europe/

it's for arduino and i don't know if it's good for STM too. you will tell me this.

bye thank you

    This topic has been closed for replies.

    6 replies

    Ons KOOLI
    Visitor II
    May 28, 2021

    Hi @arivel1​ ,

    And welcome to ST Community ! =)

    ST offers everything necessary to do the projects you listed.

    With the STM32Cube, you can find a set of tools and embedded software bricks available free of charge to enable fast and easy development on the STM32 platform which simplifies and speeds up developers’ work.

    ST offers a lot of examples and applications that can help you to start; for example you can refer to the RTC_Alarm available on the FW package correspondent to the MCU/Board you want to work with. You can also refer to the audio applications offered by ST that are available in the FW.

    I think an STM32H7 discovery board can respond to all what you are looking for (it is only a proposition based on what you described but you can choose what you want). Most of ST discovery boards that contain a screen come with an interesting demo that you will find so useful for you.

    I also recommend to use TouchGFX, which will help you to design your screens with simple ways.

    Please see TouchGFX Demo on STM32H750B-DK and ST TouchGFX Demo Video

    For more videos: visit this link.

    I really hope this is helpful!

    Best Regards,

    Ons.

    arivel1
    arivel1Author
    Associate
    May 31, 2021

    is there a guide, a tutorial, in text format?

    Ons KOOLI
    Visitor II
    May 31, 2021

    Hi @arivel1​ ,

    You can refer to these application notes : AN4759 & AN4309.

    Best Regards,

    Ons.

    arivel1
    arivel1Author
    Associate
    May 31, 2021

    no sorry I was referring to the STM32Cube software

    arivel1
    arivel1Author
    Associate
    October 23, 2021

    I tried but for me it is too complicated.

    is there anyone willing to do it on payment ?

    arivel1
    arivel1Author
    Associate
    November 5, 2021

    I found some programs on the net, each one performs its function.

    for example i found the one for solar-legal change but for arduino and another program that sends audio to the I2S output.

    the question is: if I find other programs that perform the remaining functions, can I assemble them together?

    once this is done, can you help me to correct any errors?