Read our guidelines, share your thoughts about your community experience, and explore community insights.
Most recent activity
When a link is given to a particular post and the post has a file attached, two horizontal lines appear under the small file icon.https://community.st.com/t5/stm32-mcus-products/stm32f4-hardfault/m-p/604656/highlight/true#M226598As can be seen in the picture, the lines do not appear on other posts with file attachments. And, if one takes a link to the second post of the two, then the lines appear on the second post but not on the first one.
what-the-huck-is-that?!!! my dear ST!you think you software is well-designed, works stable and correctly not because it isn't FULL OF BUGS and was never created DEFECTIVE-BY-DESIGN, but because you are not getting the feedback.the Suck-o-Sales era has become... and you know what? - there are Chinese guys, producing replacements of ST MCUs.am i really right in buying yours?
JW
The "member callout bubble" remained stuck even after having made the post i.e. editor pane closed. It overlaps the post and scrolls together with it.Oh yes, reload "fixes" it, but ain't it a hillarious fail?JW
I got a notification, where actually there is NO answer!
Here's a thread:https://community.st.com/t5/stm32-mcus-products/nucleo-144-no-pins-in-cn11-and-cn12/m-p/612257Here's what the top of the page looks like. Note that the "accepted solution" shown doesn't have the green border, and doesn't appear to have been selected by the OP as the answer.Another solution below does have the green border and appears to be the correct "solution" per the OP.Note that the "Go to solution" link goes to the incorrect solution.
Hi, @Amel NASRI ,now, that the Ideas are gone, can we please have back the annual Wishlist thread?Thanks,Jan@Amelie ACKERMANN, @Lina_DABASINSKAITE , @Laurids_PETERSEN
This page Free Arm Keil MDK for STM32C0, STM32F0, STM32L0 and STM32G0 - C/C++ Compiler, IDE/Debugger, CMSIS components, RTOS for STM32C/F/L/G/0 - STMicroelectronics and the rabbit hole it goes down is too deep and unnecessarily difficult to navigate to find the PSN / LIC that's needed Turns out it's here Keil MDK | Keil MDK for STM32 – Arm Developer (arm-sc10xp1-pre-prod-cd.azurewebsites.net)And the Product Serial Number good until December 2032 is 4RMW3-A8FIW-TUBLG
We should have a room for notable quotes somewhere.This one made my day today: There is an issue somewhere, but if we always fall back to "well it works on an identical configuration" we don't advance the ball.-- @TDK
Actually, there is text next to that icon. And it even highlights upon mouse hover, making it marginally readable.Congrats to modern feel and look.JWPS. Text ought to be BLACK and WHITE. Leave modern feel and look to marketing material. We actually need to read this.
How can I get a more Classic Forum view, say just the Subject/Title, like an email client, where I can see 50 posts, perhaps 25 to the physical height of the screen? Posting to main "Board" as there isn't a selection for "About Forum" or more appropriate venue. Also no appropriate "Label"
Dragged a mouse accidentally over this post down there. Pressed at least one or both of the left/right mouse buttons at the same time. The screenshot has not been modified...The only interaction with the page, that still works:Scrolling. Also middle (wheel) click does only scrolling anywhere on a page and doesn't open links in a new tab, like it normally does.Ctrl+A (select all). The left click cancels the "select all", but cannot do anything else.Right click.Happened on a Vivaldi browser, which is Chromium/Blink based.
Yesterday, the thread view changed from showing about 3 threads per page to about 10 or so by only showing the title and not a preview of the contents. It is so much better. It's something that has been suggested by myself and others multiple times. So thanks for that.I'm hoping this was a deliberate change and won't be changing back.I think it also shows users that the title matters so they should be more incentivized to pick a good title rather than something like "XYZ doesn't work". Glad we don't have many posts with the entire post in the title anymore.Progress.
I have to make this post, as it is really annoying for me. I would like to use other words for this, but im trying to stay professional about this!Its already bad enough, when your login expires after only like 1-2 hours. Now why on earth would a password expire, when i tried 4 times??? I am happy to wait an increasing few seconds after each fail. I guess when it expires, i cant reset it to the old one!?!Is it really necessary for the password, to have a requirement for 12 characters? And all the other requirements? What comes next? Two factor authentication?This is not a banking account!
When looking at a subforum, on the right side there are many labels available. For example, for the "Embedded software (MCUs)", the list starts with a label "ADC". But, when creating or editing a topic, there are just 9 labels available starting with "STM32Cube MCU Packages". Adding a valid label manually, ends up with an error message: "The following labels are not available here: ...".
This is not a bug of the forum engine, but of the main ST web server! Let's open the following link:https://www.st.com/resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdfBy default on a Chromium/Blink based browsers it just opens a PDF file in a tab, but on Firefox it offers a file download. The cause of the difference is the HTTP Content-Disposition header. Look at what a valid syntax is and what the ST web server returns:content-disposition: /resource/en/application_note/an2606-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdfThis is a nonsense, which doesn't conform to the HTTP standard! Apparently the Chromium/Blink based browsers interpret such a nonsense as "inline", but the Firefox interprets it as "attachment". Read the following link for a more detailed explanation and an override workaround for Firefox:https://support.mozilla.org/en-US/questions/1387228
If one takes a link to a specific post, then the posts, which had been moved from other topics, show the title of their respective original topic.Original post (OK)Moved post (wrong title):Also, as I have reported previously, adding a "Re: " in front of the title, is an anachronism from the e-mail "traditions" and is not only useless, but also worsens the usability.
I hate when i have to come on this site for resources.Now i need to download https://www.st.com/en/embedded-software/stsw-wise-studio.htmlBut it just does'nt work as i keep being repeated I have to log in but i already am. I tried switching browser.Nothing works, and i've lost so much time already :(Stress and money loss for me, thank you.
Hi, Just wondering what happened to the "My Creations" where people could post entire projects? I have a couple of projects that solve some of the problems people have had such as WiFi for the STM32H7B3I-DK, using one pulse timers, and have posted one or two projects in the past, but they have disappeared.Best regardsRob
Pictures got lost during migration, too, for example: JW
I would like to change my account password, but I can't find how to do it...Under my account and my settings I can't find any option/command for this purpose.
https://community.st.com/t5/stm32-mcus-products/uart-receive-issue/m-p/602914/highlight/true#M226105How am I supposed to view a code at a longer lines, which have to be scrolled to the right, if the horizontal scrollbar is 8 screens down? And such a long blocks are not usable anyway. There is a simple solution for both of these issues - limit the maximum vertical size of the code blocks. The size should definitely be smaller than the average screen size. Probably some 30-40 visible lines of code are fine.
Duplicating posts, uploading the same files multiple times, even replying to themselves - nothing will stop "alternatively gifted" users from abusing that button and creating a mess.https://community.st.com/t5/stm32-mcus-products/stm32f4-hardfault/m-p/604656/highlight/true#M226598The whole idea of "in response to ..." is a leftover from the broken threaded mode design. The Reply button on every post, the "in response to ..." line and the whole threaded mode should be removed and instead a proper actually useful quoting should be implemented.
and have certain freedom of speech here? ))
To add insult to injury, in preview, the text is not shortened:I strongly suggest to invite Khoros' "experts" to experience the shame personally here.JW
ST Community highlights – April to June 2026
Already have an account? Login
No account yet? Create an account
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.