Skip to main content
Jawad Waheed
Associate II
May 2, 2018 8:12 AM UTC
Question

Changing Language from Korean to English for Display (PSD913F2)

Posted on May 02, 2018 at 10:12

I am running a machine (steam generator) that has a control system with LCD display based on DS80C320 microcontroller, and PSD913F2 Flash ISP. The display language is in Korean, and I want to convert that into English. How can I perform the conversion of the langauge?  

    This topic has been closed for replies.

    9 replies

    AvaTar
    Senior III
    May 2, 2018 9:14 AM UTC
    Posted on May 02, 2018 at 11:14

    The DS80C320 is a 8051-compatible MCU, not sure if are in the proper forum, at the proper vendor.

    The display language is in Korean, and I want to convert that into English. How can I perform the conversion of the langauge?

    Considering the MCU and the assumed environment, by:

       -  translating the Korean texts

       -  rewrite the application

    Jawad Waheed
    Associate II
    May 2, 2018 12:10 PM UTC
    Posted on May 02, 2018 at 12:10

    Thanks for your reply.. how can I access that korean texts stored in MCU?

    meyer.frank

    Jawad Waheed
    Associate II
    May 2, 2018 2:38 PM UTC
    Posted on May 02, 2018 at 14:38

    There is this LCD Module with Toshiba T6963C Controller, which is bus connected to a PCB that has a ST PSD913F2-90J and a DS80C320 Microcontroller embedded on it, and only a JTAG connector IEEE1149.1 ( enabling only 4 pins : TDO, TDI, TCK, TMS) ... as the display is in Korean, the LCD controller T6963C is using a custom External Memory to read characters, most probably ST PSD913F2-90J, so my question was how to access this PSD913F2 and change where ever that Korean Display data is stored into English. I dont have any firmware binary, but want to access and amend it. 

    Tesla DeLorean
    Guru
    May 2, 2018 3:02 PM UTC
    Posted on May 02, 2018 at 17:02

    Thread seemed to have forked over to here

    https://community.st.com/0D50X00009XkWO0SAN

     
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Jawad Waheed
    Associate II
    May 2, 2018 5:34 PM UTC
    Posted on May 02, 2018 at 17:34

    it seemed more pertinent there..