Skip to main content
vrouesnel
Associate II
May 11, 2015
Question

Does the HAL support MMC?

Posted on May 12, 2015 at 01:12

So in `SD_PowerON` there is a comment at the bottom that says `/* else MMC Card */`. `hsd->CardType` is never set to `MULTIMEDIA_CARD` which is defined in `stm32f4xx_hal_sd.h`, and read in `HAL_SD_WideBusOperation_Config`.  I have generated a project in the Cube and changed the `Mode` of `SDIO` to `eMMC 4 bits wide`, but it doesn't seem any different to the SD version.  Here is the function for reference:-  /**
* @brief Enquires cards about their operating voltage and configures clock
* controls and stores SD information that will be needed in future
* in the SD handle.
* @param hsd: SD handle
* @retval SD Card error state
*/
static HAL_SD_ErrorTypedef SD_PowerON(SD_HandleTypeDef *hsd)
{
SDIO_CmdInitTypeDef sdio_cmdinitstructure; 
__IO HAL_SD_ErrorTypedef errorstate = SD_OK; 
uint32_t response = 0, count = 0, validvoltage = 0;
uint32_t sdtype = SD_STD_CAPACITY;
/* Power ON Sequence -------------------------------------------------------*/
/* Disable SDIO Clock */
__HAL_SD_SDIO_DISABLE(); 
/* Set Power State to ON */
SDIO_PowerState_ON(hsd->Instance);
/* 1ms: required power up waiting time before starting the SD initialization 
sequence */
HAL_Delay(1);
/* Enable SDIO Clock */
__HAL_SD_SDIO_ENABLE();
/* CMD0: GO_IDLE_STATE -----------------------------------------------------*/
/* No CMD response required */
sdio_cmdinitstructure.Argument = 0;
sdio_cmdinitstructure.CmdIndex = SD_CMD_GO_IDLE_STATE;
sdio_cmdinitstructure.Response = SDIO_RESPONSE_NO;
sdio_cmdinitstructure.WaitForInterrupt = SDIO_WAIT_NO;
sdio_cmdinitstructure.CPSM = SDIO_CPSM_ENABLE;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */
errorstate = SD_CmdError(hsd);
if(errorstate != SD_OK)
{
/* CMD Response Timeout (wait for CMDSENT flag) */
return errorstate;
}
/* CMD8: SEND_IF_COND ------------------------------------------------------*/
/* Send CMD8 to verify SD card interface operating condition */
/* Argument: - [31:12]: Reserved (shall be set to '0')
- [11:8]: Supply Voltage (VHS) 0x1 (Range: 2.7-3.6 V)
- [7:0]: Check Pattern (recommended 0xAA) */
/* CMD Response: R7 */
sdio_cmdinitstructure.Argument = SD_CHECK_PATTERN;
sdio_cmdinitstructure.CmdIndex = SD_SDIO_SEND_IF_COND;
sdio_cmdinitstructure.Response = SDIO_RESPONSE_SHORT;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */ 
errorstate = SD_CmdResp7Error(hsd);
if (errorstate == SD_OK)
{
/* SD Card 2.0 */
hsd->CardType = STD_CAPACITY_SD_CARD_V2_0; 
sdtype = SD_HIGH_CAPACITY;
}
/* Send CMD55 */
sdio_cmdinitstructure.Argument = 0;
sdio_cmdinitstructure.CmdIndex = SD_CMD_APP_CMD;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */
errorstate = SD_CmdResp1Error(hsd, SD_CMD_APP_CMD);
/* If errorstate is Command Timeout, it is a MMC card */
/* If errorstate is SD_OK it is a SD card: SD card 2.0 (voltage range mismatch)
or SD card 1.x */
if(errorstate == SD_OK)
{
/* SD CARD */
/* Send ACMD41 SD_APP_OP_COND with Argument 0x80100000 */
while((!validvoltage) && (count < 
SD_MAX_VOLT_TRIAL
))
{
/* SEND CMD55 APP_CMD with RCA as 0 */
sdio_cmdinitstructure.Argument
= 
0
;
sdio_cmdinitstructure.CmdIndex
= 
SD_CMD_APP_CMD
;
sdio_cmdinitstructure.Response
= 
SDIO_RESPONSE_SHORT
;
sdio_cmdinitstructure.WaitForInterrupt
= 
SDIO_WAIT_NO
;
sdio_cmdinitstructure.CPSM
= 
SDIO_CPSM_ENABLE
;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */
errorstate = SD_CmdResp1Error(hsd, SD_CMD_APP_CMD);
if(errorstate != SD_OK)
{
return errorstate;
}
/* Send CMD41 */
sdio_cmdinitstructure.Argument = SD_VOLTAGE_WINDOW_SD | sdtype;
sdio_cmdinitstructure.CmdIndex = SD_CMD_SD_APP_OP_COND;
sdio_cmdinitstructure.Response = SDIO_RESPONSE_SHORT;
sdio_cmdinitstructure.WaitForInterrupt = SDIO_WAIT_NO;
sdio_cmdinitstructure.CPSM = SDIO_CPSM_ENABLE;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */
errorstate = SD_CmdResp3Error(hsd);
if(errorstate != SD_OK)
{
return errorstate;
}
/* Get command response */
response = SDIO_GetResponse(SDIO_RESP1);
/* Get operating voltage*/
validvoltage = (((response >> 31) == 1) ? 1 : 0);
count++;
}
if(count >= SD_MAX_VOLT_TRIAL)
{
errorstate = SD_INVALID_VOLTRANGE;
return errorstate;
}
if((response & SD_HIGH_CAPACITY) == SD_HIGH_CAPACITY) /* (response &= SD_HIGH_CAPACITY) */
{
hsd->CardType = HIGH_CAPACITY_SD_CARD;
}
} /* else MMC Card */
return errorstate;
}

Note: this post was migrated and contained many threaded conversations, some content may be missing.
    This topic has been closed for replies.

    37 replies

    Nemui Trinomius
    Associate II
    January 20, 2017
    Posted on January 20, 2017 at 02:13

    Dear all,

    I found  MMC(and eMMC) support added on newest CubeF7V1.6.0!

    http://www.st.com/en/embedded-software/stm32cubef7.html

     

    And sdcard HAL driver was revised overall from former one.

    Gid Rid
    Associate III
    February 3, 2017
    Posted on February 03, 2017 at 12:09

    Dear All,

    I'm just getting into this problem too as I need to support an eMMC with the STM32F7. What I have found so far:

    1. The drivers in STM32CubeF7 1.6.0 seem to be the same as what is in STM32CubeMX 4.19.0

    2. There is a HAL 'driver' for MMC in those libraries, but you cannot enable it in the GUI.

    3. There is no user level layers between the HAL MMC driver and FATfs, i.e. no 'bsp_driver_mmc.c' or 'mmc_diskio.c'.

    4. The HAL driver for MMC does not support memories over 2GB.

    5. The HAL driver for MMC may not ever have been used or even compiled, as it has inconsistencies in function names.

    I am currently working my way through all this. I have had some success by writing the missing bits, but still have some issues to fix. Card initialisation seems to work stepping through with the debugger but fails at full speed, and I also get errors when trying to write a file.

    Gid Rid
    Associate III
    May 21, 2018
    Posted on May 21, 2018 at 11:50

    Nemui Trinomius is the only code I found that works. There is hope that the STM32H7 supporting eMMC 4.5 will result in improvements to the HAL library and CubeMX.