Power management

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Signal sniffer

Hi everyone.I have a position encoder connected to a motor drive. The encoder transmit every 0.1ms a 73-bit data package using a protocol called EnDat 2.2 to the drive. The clock frequency is set to 5MHz, meaning one bit is 0.2 microsecond. Now I wan...

0690X00000A9ZljQAF.png
huy.pham by Associate
  • 572 Views
  • 2 replies
  • 0 kudos

Use the L6563s to design a dc power

Posted on June 28, 2018 at 10:24Hi?I use the L6563S to design a 200W DC power.I just wanted to know how the L6563s to start working .I don't know the effect of diode D0 betweeninductanceT1  and capacitorC0.What it needs to work normally form the sta...

0690X0000060BvHQAU.png