Skip to main content
embvis
Associate III
November 9, 2017
Solved

STM32H7 nucleo USB FS CDC

  • November 9, 2017
  • 19 replies
  • 7991 views
Posted on November 09, 2017 at 10:37

Hi,

I am trying to start with USB CDC on stm32h7. I create new project with CubeMx + STM32Cube_FW_H7_V1.1.0 (cubemx file attached). After compile usb device doesnt appear on the system.

Regards

Mike

#stm32h743 #virtual-comport-stm32 #cdc #stm32h7 #usb-device #usb-fs-cdc
This topic has been closed for replies.
Best answer by Marina Brener
Posted on November 09, 2017 at 16:12

Hi Mikolaj,

I had the same problem, this function solved it : 

HAL_PWREx_EnableUSBVoltageDetector() .

Please add this function call to usb_device.c file like this.

void MX_USB_DEVICE_Init(void)

{

/* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */

/* USER CODE END USB_DEVICE_Init_PreTreatment */

/* Init Device Library,Add Supported Class and Start the library*/

USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);

USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC);

USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS);

USBD_Start(&hUsbDeviceFS);

/* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */

HAL_PWREx_EnableUSBVoltageDetector();

/* USER CODE END USB_DEVICE_Init_PostTreatment */

}

Hope it helps!

Marina

19 replies

Marina Brener
Marina BrenerBest answer
Associate III
November 9, 2017
Posted on November 09, 2017 at 16:12

Hi Mikolaj,

I had the same problem, this function solved it : 

HAL_PWREx_EnableUSBVoltageDetector() .

Please add this function call to usb_device.c file like this.

void MX_USB_DEVICE_Init(void)

{

/* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */

/* USER CODE END USB_DEVICE_Init_PreTreatment */

/* Init Device Library,Add Supported Class and Start the library*/

USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);

USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC);

USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS);

USBD_Start(&hUsbDeviceFS);

/* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */

HAL_PWREx_EnableUSBVoltageDetector();

/* USER CODE END USB_DEVICE_Init_PostTreatment */

}

Hope it helps!

Marina

Handzic.Dirk
Associate III
May 8, 2018
Posted on May 08, 2018 at 11:12

Thank you for sharing! I am working on a recently designed STM32H743II board and faced the same issue! Even the latest CubeMX4.25.0 and STM32H7Cube 1.2 dont fix this issue.

Next problem I am facing is to detect a USB memory stick attached to the USB HS HOST port using the MSC class. The USBH_Process() is always in the HOST_IDLE state.

Best regards

Dirk

ST Technical Moderator
May 8, 2018
Posted on May 08, 2018 at 11:39

Hello

Handzic.Dirk

,

ST team is aware about the issue ofmissing call to HAL_PWREx_EnableUSBVoltageDetector( ) and should fix this limitation in the coming release, but all

depends on releases planning and expected fixes or new features to embed.

It should be better to start a new discussion for new issue with more details even if the topic is the same.

Best Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
embvis
embvisAuthor
Associate III
November 12, 2017
Posted on November 12, 2017 at 02:34

Its now workingk. Thank you Marina.

ST Technical Moderator
November 16, 2017
Posted on November 16, 2017 at 15:40

Hello,

Thank you to share this issue. I raised it internally to the appropriate team for work and fix it.

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Andrew Ivanov
Associate II
November 29, 2017
Posted on November 29, 2017 at 08:34

May be you know how to resolve, I worked with nucleo144 board (stm32f767) and I had some problem. Windows define board how unkown usb device. But Keil debuger stopped in irq handler 'void OTG_FS_IRQHandler(void)'. May be I dont`t initialize any option.

Andrei Chichak
Lead
December 11, 2017
Posted on December 11, 2017 at 18:38

I'm having this same issue with my nucleo144 (F767) board.

I get interrupts going to OTG_FS_IRQ_Handler, which calls HAL_PCD_IRQHandler.

BUT, none of the functions hooked using USBF_Interface_fops_FS are ever called.  CDC_Init_FS never gets called.

I have been tracing the code for the last week and  the functions get hooked into hpcd-> pData properly, but I can't figure out where the HAL_PCD routines actually call the routines that are pointed at.

I tried putting in the call to

HAL_PWREx_EnableUSBVoltageDetector

, which didn't make sense, 

but it doesn't seem to exist in F7 HAL version 1.8.0.

It's like the CDC/PCD connection is broken in 1.8.0.

Andrei

Marina Brener
Associate III
December 12, 2017
Posted on December 12, 2017 at 21:08

Hi Andrei,

I was using this function because the usb voltage on stm32h7 comes from VDD33 voltage level detector.

So the code is actually:

void HAL_PWREx_EnableUSBVoltageDetector(void)

{

  /* Enable the USB voltage detector */

  SET_BIT(PWR->CR3, PWR_CR3_USB33DEN);

}

Is stm32f767 has a USB regulator that needs to be enabled?

0690X00000609CPQAY.png
esukh
Associate II
August 16, 2018

HI, I have similar issue, but

HAL_PWREx_EnableUSBVoltageDetector() doesn't do the trick for me, my bet is incorrect codebase generated by stm32cubeMX 4.26 + FW 1.3

Is there anyone who deal with that problem?

Actually usb33den bit doesn't set after function call, in debugger at least.

JSmit.15
Visitor II
September 28, 2018

I am using PB13,PB14,PB15 for USB host connectivity and PF2,PF3 for USB_HOST_PWRON and USB_HOST_OVERCURR using a STMPS2141 to provide power to the host connector. 

https://www.brotherprintersupportnumber.com/brother-printer-setup/

Papayaved
Visitor II
June 7, 2019

I have same problem with NUCLEO STM32H743ZI Virtual Com Port - I can not open port on PC

I have Nucleo STM32H743ZI board. I'm using CubeMX HAL (I tried several versions) and TrueStudio. "Virtual COM port" appearances in Windows 10 (I tried default Windows driver and ST driver) but I can not open port. My C# program write me "The parameter is incorrect" when I try open it:

SerialPort port = new SerialPort("COM8", 9600, Parity.None, 8, StopBits.One);
port.Open(); // System.IO.IOException: 'The parameter is incorrect.'

same message writes me program Realterm, PuTTY do nothing and "Tera Term" program works correct - I can send and receive data to my MCU program.

May anyone know what is it?

In my C# program and in terminal programs I use same parameters

Papayaved
Visitor II
June 7, 2019

STM32H743ZI USB FullSpeed Virtual Com Port: 'Com port parameter is incorrect'

For data exchange with MCU on Windows 10 I use C function: fopen("COM6", "r+"), fwrite, fgetc, fclose, - without COM port parameters and it's work. But if I use C++ Qt or C# libraries, when I try to open the COM port I catch exception 'The parameter is incorrect'. Same exception I catch in PuTTY and RealTerm programs. I tried setting various parameters. I think USB device cannot accept COM port parameters from PC. I used Nucleo and my board with same result.

I use CubeMX 5.2.1 and FW 1.4.0. If I use CubeMX 4.27.0 and FW 1.3.2 PC is not found USB device.

Also USB description has error in field bDeviceSubClass in FW 1.4.0 and FW 1.3.2.

Microsoft UsbView program:

     ===>Device Descriptor<===

bLength:             0x12

bDescriptorType:         0x01

bcdUSB:             0x0200

bDeviceClass:           0x02 -> This is a Communication Device

bDeviceSubClass:         0x02

*!*ERROR: bDeviceSubClass of 2 is invalid

bDeviceProtocol:         0x00

bMaxPacketSize0:         0x40 = (64) Bytes

idVendor:            0x0483 = STMicroelectronics

idProduct:           0x5740

bcdDevice:           0x0200

iManufacturer:          0x01

   English (United States) "STMicroelectronics"

iProduct:             0x02

   English (United States) "STM32 Virtual ComPort"

iSerialNumber:          0x03

   English (United States) "383A34463137"

bNumConfigurations:        0x01

Papayaved
Visitor II
June 7, 2019

 ---===>Open Pipes<===---

 ===>Endpoint Descriptor<===

bLength:              0x07

bDescriptorType:          0x05

bEndpointAddress:         0x82 -> Direction: IN - EndpointID: 2

bmAttributes:           0x03 -> Interrupt Transfer Type

wMaxPacketSize:         0x0008 = 0x08 bytes

bInterval:             0x10

 ===>Endpoint Descriptor<===

bLength:              0x07

bDescriptorType:          0x05

bEndpointAddress:         0x01 -> Direction: OUT - EndpointID: 1

bmAttributes:           0x02 -> Bulk Transfer Type

wMaxPacketSize:         0x0040 = 0x40 bytes

bInterval:             0x00

 ===>Endpoint Descriptor<===

bLength:              0x07

bDescriptorType:          0x05

bEndpointAddress:         0x81 -> Direction: IN - EndpointID: 1

bmAttributes:           0x02 -> Bulk Transfer Type

wMaxPacketSize:         0x0040 = 0x40 bytes

bInterval:             0x00

  ---===>Full Configuration Descriptor<===---

 ===>Configuration Descriptor<===

bLength:              0x09

bDescriptorType:          0x02

wTotalLength:          0x0043 -> Validated

bNumInterfaces:          0x02

bConfigurationValue:        0x01

iConfiguration:          0x00

bmAttributes:           0xC0 -> Self Powered

MaxPower:             0x32 = 100 mA

 ===>Interface Descriptor<===

bLength:              0x09

bDescriptorType:          0x04

bInterfaceNumber:         0x00

bAlternateSetting:         0x00

bNumEndpoints:           0x01

bInterfaceClass:          0x02 -> This is Communications (CDC Control) USB Device Interface Class

bInterfaceSubClass:        0x02

bInterfaceProtocol:        0x01

iInterface:            0x00

 -> This is a Communications (CDC Control) USB Device Interface Class

 ===>Descriptor Hex Dump<===

bLength:              0x05

bDescriptorType:          0x24

05 24 00 10 01 

 -> This is a Communications (CDC Control) USB Device Interface Class

 ===>Descriptor Hex Dump<===

bLength:              0x05

bDescriptorType:          0x24

05 24 01 00 01 

 -> This is a Communications (CDC Control) USB Device Interface Class

 ===>Descriptor Hex Dump<===

bLength:              0x04

bDescriptorType:          0x24

04 24 02 02 

 -> This is a Communications (CDC Control) USB Device Interface Class

 ===>Descriptor Hex Dump<===

bLength:              0x05

bDescriptorType:          0x24

05 24 06 00 01 

 ===>Endpoint Descriptor<===

bLength:              0x07

bDescriptorType:          0x05

bEndpointAddress:         0x82 -> Direction: IN - EndpointID: 2

bmAttributes:           0x03 -> Interrupt Transfer Type

wMaxPacketSize:         0x0008 = 0x08 bytes

bInterval:             0x10

 ===>Interface Descriptor<===

bLength:              0x09

bDescriptorType:          0x04

bInterfaceNumber:         0x01

bAlternateSetting:         0x00

bNumEndpoints:           0x02

bInterfaceClass:          0x0A -> This is a CDC Data USB Device Interface Class

bInterfaceSubClass:        0x00

bInterfaceProtocol:        0x00

iInterface:            0x00

 ===>Endpoint Descriptor<===

bLength:              0x07

bDescriptorType:          0x05

bEndpointAddress:         0x01 -> Direction: OUT - EndpointID: 1

bmAttributes:           0x02 -> Bulk Transfer Type

wMaxPacketSize:         0x0040 = 0x40 bytes

bInterval:             0x00

 ===>Endpoint Descriptor<===

bLength:              0x07

bDescriptorType:          0x05

bEndpointAddress:         0x81 -> Direction: IN - EndpointID: 1

bmAttributes:           0x02 -> Bulk Transfer Type

wMaxPacketSize:         0x0040 = 0x40 bytes

bInterval:             0x00