ST10F252-ABG
I know that this IC: ST10F252-ABG is old, but is there any cross or direct replacement for it?Thanks,Byron
I know that this IC: ST10F252-ABG is old, but is there any cross or direct replacement for it?Thanks,Byron
Do you have a data sheet for this product? Has this product been discontinued? Is there a reference for alternative part numbers
Hi,For some time now I was using cheap bluepill and stm32f030-demo boards to debun my project with st-link probes. It all works perfect. But recently the stmf030 become too small, so I decided to replace it with stm32f070 (same tssop20 package as ori...
Hi allI have difficulty to find data sheet of this part BEXY Z531 thank you for any respondBest Regard
Hello,Hello,I am using STLINK V2 & using SWD for flashing. Please can you confirm if Tag-Connect ARM20-CTX & TC2030-IDC are compatible to STLINK V2.
Hi, When I connect a digital radio via the USB cable, Device Manager should show under USB: STM Device in DFU mode. However, it doesn't. Instead, I have an Other Devices: Digital Radio in USB mode, with a yellow triangle with black exclamation point....
Hi all and good time can U help me please?i'm confused about this part with the (UM smd code),i searched a lot on google and but i found only 2 parts with this smd code... (zener diode and tvs diode) !!my first find --> zener diode Bzx84j-C5V6 SOD-32...
Hello community,i have trouble to identify a defect power semiconductor from ST.The package is TO-220 and is marked with "GF309VW" and the ST-Logo. Can anyone identfiy the device?Thanks in advance!
I have the following questions and need help:1. Can this transistor be used at a frequency of 900kHz? Can it only be used in frequency bands above 1MHz?2. The data sheet provides a test circuit under 30MHz conditions. We do not fully understand the f...
What steps are required to set stwlc98 to TX mode?If you set 0x0020 to 01, 0x000E becomes 03.However, AC1 and AC2 do not cause burst oscillation.The Optional (TX mode only) circuit is on the board, and VOUT is connected to 5V.