STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32L452CEU6 usb doesnt work with Samsung GalaxyTab A8

I have a board design based on stm32L452 , USB gets recognized on a windows PC and I can talk to the device over any software like putty and a Test software sees the com port and can to the device. However in Android (Iam using samsung  GalaxyTab A8)...

anees by Associate II
  • 4786 Views
  • 32 replies
  • 0 kudos

DAC trigger by HRTIM

Hi, I need to trigger DAC1 and DAC2 from HRTIM Timer A on a STM32G474. I have set the DAC Sync option inside the HRTIM Timer A settting to generate a DACTrigOut1 event that triggers my DAC1. But DAC has a separate Trigger event that also works for DA...

berait by Associate II
  • 84 Views
  • 0 replies
  • 0 kudos

sbsfu boot image not found

hi,i use sbsfu bootloader, the problem was the boot don't found the image.i used Ymodem to send image but the same think .as montionned in the image bellow. 

tawfik_0-1715098023077.png
tawfik by Associate
  • 112 Views
  • 0 replies
  • 0 kudos

Resolved! I2C start condition not generates ( SB flag is never set )

I'm working on stm32f103 I2C peripheral. I've one stm32f103 master and another stm32f103 slave. The master should send some text to the slave, but start condition never generates. The BUSY flag is set as soon as the peripheral is enable and the progr...

ASeyo by Associate II
  • 628 Views
  • 2 replies
  • 0 kudos

does STM32H563ZIT6 has support for OTFDEC

I'm using NUCLEOH56ZI board which consists of STM32H563ZIT6 controller.I'm checking, if there is any provision to encrypt the data/program on external FLASH.in the stm32h563/573 reference manual ,i see OTFDEC is a feature provided for this purpose.bu...

shii by Associate II
  • 230 Views
  • 5 replies
  • 1 kudos

Watchdog not wakeup from the STOP mode occasionally

My STM32L051C8T6 board encountered a very strange phenomenon. It occasionally failed to wake up from the STOP mode, although the IWDG was enabled.I am using Zephyr RTOS, but do not enable Zephyr's power management, and use the following peripherals:1...

guojing by Associate
  • 169 Views
  • 2 replies
  • 1 kudos

Error Target MCU stm32f401cd

Salut la communauté, J'ai créé une carte électronique permettant de visualiser l'état de la batterie d'un ULM. J'ai utilisé le microcontrôleur STM32F401CD, et j'avais initialement prévu d'utiliser uniquement l'horloge interne HSI du MCU, donc je n'ai...

yassir by Associate III
  • 728 Views
  • 44 replies
  • 9 kudos

CAN Filter ExtID

Hi,I want to setup the CAN filter but I don't understand how to do so.I have made lot of test but nothing work fine.I want to have only message 0x18FF01D0, 0x18FF02D0, 0x18FF03D0, 0x18FF05D0, 0x18FF07D0, 0x18FF0CD0 and a stdID 0x401.To test to have o...

AJouv by Associate II
  • 758 Views
  • 7 replies
  • 0 kudos
Labels