STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STlink different pinout information

Hello,I'm developing a customized board with STM32H723ZGT6, and I need to prepare it to program the uC, so I'm placing a connector to conect the STlink V2 or V3. Looking for the documentation I have diferent information about the programmer pinout. I...

zpedro_0-1741800128192.png zpedro_1-1741800175148.png
zpedro by Associate
  • 239 Views
  • 1 replies
  • 0 kudos

ADC - watchdog

@Amel NASRI @Tesla DeLorean Hi! I have a question about the ADC WD. I am trying to use it, being triggered by a touchscreen, I have set it as follow: static void MX_ADC1_Init(void){/* USER CODE BEGIN ADC1_Init 0 *//* USER CODE END ADC1_Init 0 */ADC_A...

Resolved! STM32 Black Pill not detected by ST-Link

I Recently bought a STM32F411CEU6 . It was working fine till i shorted two pins by mistake.The STM IDE says no target found when i try to upload the code .Only the power LED turns on but the USER LED doesn't.(The ST-Link still detects my Blue pill pr...

Resolved! STM32F103C8T6 Blue Pill project

First and foremost, as of this point I know virtually nothing about these MC's but through this project, I'm hoping to learn. What I'd like to get some assistance on is just a few basic pointers and perhaps direction so that I'm not chasing my tail.T...

jw11432 by Associate
  • 1279 Views
  • 3 replies
  • 0 kudos

Resolved! id is not recognized , stm32f103c8

i have this problem https://community.st.com/t5/stm32-mcus-boards-and-hardware/error-in-initializing-st-link-device-reason-18-could-not-verify/td-p/314096 that ,  attach chip  photo  it doesn't look like a counterfeit chip   Open On-Chip Debugger 0....

stm32f103c8_no_id.jpeg