Skip to main content
Associate II
May 19, 2026
Question

Bif fat ugly bug in STM32G0B1 bootloader

  • May 19, 2026
  • 0 replies
  • 107 views

The STM32G0B1 has a very ugly bug in the bootloader.

When I have a write protection on a flash memory area:

WRP1A_STRT = 0x0 --> 0x08000000
WRP1A_END = 0x1 --> 0x08000800

and then I upload a new firmware to this area the firmware will not be written, because this area is write protected.
This is correct.

But it is a horrible bug that I send a USB control request with

Request.Function=URB_FUNCTION_CLASS_INTERFACE;
Request.Direction=VENDOR_DIRECTION_IN;
Request.Request=DFU_GETSTATUS;
Request.Value=0;
Request.Index=0;
Request.Length=6;
Result = STDevice_ControlPipeRequest(hDevice, &Request, (BYTE*)pkDfuStatus);

and the buggy bootloader returns STATUS_OK (value 0) instead of STATUS_ErrorWRITE (value 3)

The user thinks that the firmware was uploaded correctly but the processor is dead because the flash memory is corrupt.