what is the smallest achievable delay in microseconds for a 16-bit and a 32-bit timer?
Hi, I want to generate a 1 microsecond (1 µs) timer interrupt on the STM32G0B1RCT6 microcontroller using its internal clock(16MHz). I am currently using a 16-bit timer to achieve a 5 microsecond delay, but I cannot achieve a 1 microsecond delay. My question is: what is the smallest achievable delay in microseconds for a 16-bit and a 32-bit timer?