Skip to main content
gerhard
Associate III
August 30, 2021
Question

What are the STM32G030J6M6 pin functions after reset

  • August 30, 2021
  • 1 reply
  • 560 views

The STM32G030J6M6 is the SO8N device.

The Datasheet lists different functions upon reset for pins 4, 5, 8

Any help appreciated

This topic has been closed for replies.

1 reply

TDK
August 30, 2021

The SWD pins (PA13/PA14) are initialized as such at reset. Others are initialized in high impedance input mode.

NRST is NRST, unless disabled in option bytes.

> The Datasheet lists different functions upon reset for pins 4, 5, 8

Where? I only see it call out PA13/PA14 (pins 7 and 8).

"If you feel a post has answered your question, please click ""Accept as Solution""."