Skip to main content
Rashedul Islam
Associate II
Nov 24, 2017 2:19 PM UTC
Solved

USART DMA IDLE State for STM32F401RETx

Posted on November 24, 2017 at 15:19

Hi All,

I was working on getting user input via keyboard over uart. The input could be varible length. To handle this issue I use HAL uart receive DMA (circualr mode). To get input and and tranfer it over uart, i got an example which actually serves my purpose fine. The example is by

pasztora

 and link is given below: <LINK NO LONGER ACTIVE>

Now I implement my task in STM32L476RG Nucelo board and it was absolutely fine

In the example mentioned above, there is code block,

if((USART2->ISR & USART_ISR_IDLE) != RESET)

{

    USART2->ICR = UART_CLEAR_IDLEF;

    /* Start DMA timer */

    dma_uart_rx.timer = DMA_TIMEOUT_MS;

 }

Well, for my client project I got a board which has STM32F401RETx. But for the 

STM32F401RETx board I dont get defined the below:

USART2->ISR

USART2->ICR

USART_ISR_IDLE

UART_CLEAR_IDLEF

My question is why those above mentioned are not defined? and what is alternative for that ?

what modiftion needs to be done for the above mentioned code block? 

For STM32L476RG

the type is defined as belwo:

/**

* @brief Universal Synchronous Asynchronous Receiver Transmitter

*/

typedef struct

{

__IO uint32_t CR1; /*!< USART Control register 1, Address offset: 0x00 */

__IO uint32_t CR2; /*!< USART Control register 2, Address offset: 0x04 */

__IO uint32_t CR3; /*!< USART Control register 3, Address offset: 0x08 */

__IO uint32_t BRR; /*!< USART Baud rate register, Address offset: 0x0C */

__IO uint16_t GTPR; /*!< USART Guard time and prescaler register, Address offset: 0x10 */

uint16_t RESERVED2; /*!< Reserved, 0x12 */

__IO uint32_t RTOR; /*!< USART Receiver Time Out register, Address offset: 0x14 */

__IO uint16_t RQR; /*!< USART Request register, Address offset: 0x18 */

uint16_t RESERVED3; /*!< Reserved, 0x1A */

__IO uint32_t

ISR

; /*!< USART Interrupt and status register, Address offset: 0x1C */

__IO uint32_t

ICR

; /*!< USART Interrupt flag Clear register, Address offset: 0x20 */

__IO uint16_t RDR; /*!< USART Receive Data register, Address offset: 0x24 */

uint16_t RESERVED4; /*!< Reserved, 0x26 */

__IO uint16_t TDR; /*!< USART Transmit Data register, Address offset: 0x28 */

uint16_t RESERVED5; /*!< Reserved, 0x2A */

} USART_TypeDef;

And for STM32F401RETx the type is defined as,

/**

* @brief Universal Synchronous Asynchronous Receiver Transmitter

*/

typedef struct

{

__IO uint32_t SR; /*!< USART Status register, Address offset: 0x00 */

__IO uint32_t DR; /*!< USART Data register, Address offset: 0x04 */

__IO uint32_t BRR; /*!< USART Baud rate register, Address offset: 0x08 */

__IO uint32_t CR1; /*!< USART Control register 1, Address offset: 0x0C */

__IO uint32_t CR2; /*!< USART Control register 2, Address offset: 0x10 */

__IO uint32_t CR3; /*!< USART Control register 3, Address offset: 0x14 */

__IO uint32_t GTPR; /*!< USART Guard time and prescaler register, Address offset: 0x18 */

} USART_TypeDef;

This topic has been closed for replies.
Rashedul Islam
Rashedul IslamBest answer
Associate II
Nov 27, 2017 1:47 PM UTC
Posted on November 27, 2017 at 13:47

Ok I have figure it out and its working now.

I used as below, 

__HAL_UART_CLEAR_IDLEFLAG(&huart1);  instead of  

//

USART1->ICR = UART_CLEAR_IDLEF;

5 replies

Tesla DeLorean
Guru
Nov 24, 2017 2:35 PM UTC
Posted on November 24, 2017 at 15:35

The F4 has an earlier USART design. The status bits would be in USART->SR, USART_FLAG_IDLE

For user input DMA is probably overkill

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Rashedul Islam
Associate II
Nov 24, 2017 3:55 PM UTC
Posted on November 24, 2017 at 15:55

Turvey.Clive.002

Thanks for you quick response.

As I am a newbi, I did not understand what you meant by '

For user input DMA is probably overkill

'.

Also

USART_FLAG_IDLE is not available. I simply made search to the whole project. Do I need any changes/modification to the cubeMX project configuration, which can add the required flags in the library??

I also edited my main post. You can check the highlighted code block which I want to use in STM32F4.

Tesla DeLorean
Guru
Nov 24, 2017 6:14 PM UTC
Posted on November 24, 2017 at 18:14

I've yet to meet a human that can type 1000 characters a second. I think this could be more trivially handled in an IRQ.

The F4 uses a different USART with different flagging and clearing methods, you should review the Reference Manual (RM0090) to understand the differences and whether your algorithm will port cleanly.

USART_FLAG_IDLE should be in stm32f4xx_hal_usart.h, you should check what modules are being flagged for inclusion in the stm32f4xx_hal_conf.h for your project.

Sorry not looking to port HAL code.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..