Skip to main content
Kamil Kisiel
Associate III
June 30, 2015
Question

Unable to program STM32373C-EVAL via JTAG or SWD. STLink works fine.

  • June 30, 2015
  • 2 replies
  • 663 views
Posted on July 01, 2015 at 01:23

I have been using a STM32373C-EVAL board and programming it via the onboard STLink. Recently we've moved towards our own hardware design and so to verify that our SWD programmer was working I was testing programming the eval board via the CN17 JTAG port in SWD mode.

The adapter I was using is an OLIMEX ARM-USB-OCD-H with the ARM-JTAG-SWD attachment and then jumper cables between the appropriate pins. Everything was working fine but at some point I accidentally connected two of the ARM-JTAG-SWD adapters to the same cable. Ever since then I've been unable to program the board via either JTAG or SWD connected to CN17, but the onboard STLink still works fine.

I'm able to connect via openocd but when performing a load I get errors such as:

Info : SWD IDCODE 0x2ba01477

Error: Failed to write memory at 0x200001cc

Error: error writing to flash at address 0x08000000 at offset 0x00000000

adapter speed: 1000 kHz

target state: halted

target halted due to debug-request, current mode: Thread 

xPSR: 0x01000000 pc: 0xfffffffe msp: 0xfffffffc, semihosting

Info : dropped 'gdb' connection

I also tried with an STM32F4Discovery as an STLink device but I get errors like:

Error: timed out while waiting for target halted

TARGET: stm32f3x.cpu - Not halted

in procedure 'reset' 

in procedure 'ocd_bouncer'

target state: halted

target halted due to debug-request, current mode: Thread 

xPSR: 0x21000000 pc: 0x08000770 msp: 0x20007fd8

semihosting is enabled

adapter speed: 1000 kHz

Error: timed out while waiting for target halted

TARGET: stm32f3x.cpu - Not halted

in procedure 'reset' 

in procedure 'ocd_bouncer'

Error: Target not halted

Error: failed erasing sectors 0 to 1

Error: flash_erase returned -304

Info : dropped 'gdb' connection

However programming with the onboard STLink USB device on the EVAL board continues to work as normal.

Does anyone have a clue as to what the problem may be? I notice in the schematic there's some zener diodes on the JTAG/SWD lines coming from the external connector. Is it possible those got damaged and are now causing communication to be unreliable? Based on the fact that the chip is still programmable via the onboard STLink I assume the problem is not there?
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    July 1, 2015
    Posted on July 01, 2015 at 03:52

    How does one disconnect the on-board ST-LINK from the JTAG header?

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    Kamil Kisiel
    Associate III
    July 2, 2015
    Posted on July 02, 2015 at 08:05

    I don't disconnect the onboard STLink, I just don't connect it to the computer with the USB cable (I power the board from the other USB port). To use the STM32F4Discovery STLink I used jumper wires to CN17.