Skip to main content
mm_it
Associate
November 21, 2011
Question

trouble STM32F103ZET6 make reset on warm up !!!

  • November 21, 2011
  • 0 replies
  • 379 views
Posted on November 21, 2011 at 22:06

Hello,

I have a very big problem. I have change the code and then when I make the board warm to 40�C..60�C, the processor make a reset.

If I revert my change, then I can warm up the procoessor like coocing and no reset is coming.

I have find the line:

Work well:

  return((UINT16)((tempCount32+2) / 4));

Work not:

  return((UINT16)((tempCount32+2) >> 2));

But: the processor do not jump into this line!!!

Then I want look about the assembler code, but when I add in the makefile:

 -Wa,-ahlms=$(addprefix $(OBJDIR), $(<:.c=.lst))

then the processor make a reset after warm up, without change vom code!

I have no idea what I have make wrong.

Compiler: Coudesourdery, -O1

After temperatur reset, in the register RCC->CSR, the upper 8 bit have ''0x14'', look like SW-Reset, no Watchdog!

After this reset, the processor start and work for some ms and make a reset again until the chip is cold.

I have test it with a lot of Boards an three PC's.

Please, help me!

My guess

is

that the

debug

unit

reset

the processor, 

because

the Status-Register RCC->CSR look like the same when I download a new program by JTAG.

Best Regards Markus

#stm32
    This topic has been closed for replies.