Skip to main content
T J
Senior III
August 2, 2018
Question

syntax is the bane of my work...

  • August 2, 2018
  • 4 replies
  • 954 views

I don't understand why this would compile and work for one project but not another...

const char Menu[40][32] = { 
 "\033[91;2mShow Menu\033[93;2m <space>", 
 "\033[0m ",
 "1 Read Flash status"
};
 
 char * ptr = &Menu; <- fails here

 [Clang IntelliSense] Warning: incompatible pointer types initializing 'char *' with an expression of type 'const char (*)[40][32]'   VS_EBrakes3F6   c:\users\nickm\documents\vs2018\ebrakesv3_f6\src\bios.c   1107   

    This topic has been closed for replies.

    4 replies

    RSonn
    Associate
    August 3, 2018

    I see a warning only. so compilation succeeded, I suppose. char * insn't const char *, so a warning is ok here. Perhaps in the other project compiler settings are more permissive with respect to warnings?​

    T J
    T JAuthor
    Senior III
    August 3, 2018

    thanks for looking in,

    yes, just a warning,

    seems to work now, not sure what fixed it :(

    but robust now...

    Danish1
    Lead III
    August 3, 2018

    Menu is an array of 40 constant C-strings, each with a maximum length of 32 characters.

    You have set ptr to the address of Menu - so ptr should be the same type as Menu.

    If you wanted to set ptr to point to the first string in Menu, then you should have said ptr = &Menu[0];

    Do you elsewhere access Menu[1], ...?

    Or to access the next menu-item, do you want to say ptr[1] or ++ptr? Because the C compiler would need to know that the size of the element pointed to by ptr is not 1 (sizeof(char)) but 32 (i.e. sizeof(char[32]) ) In which case ptr should be declared/initialised as const char (*ptr)[32] = &Menu;

    There's the const-ness as well as mentioned by roland.sonnenschein

    • Danish
    T J
    T JAuthor
    Senior III
    August 3, 2018

    I haven't seen this style before:

     const char (*ptr)[32]

    is that the next ptr++ will point to the next string ? adding 32 byte count