STM32H7x3I-EVAL2 board: free pins on the I/O extender (MFX)?
I need to hook few external signals to STM32H7x3I-EVAL rev. E, if possible without soldering or losing access to FMC, QSPI memories.
This board is much busier than Nucleo, I can find only few free pins on the default pinout.
The user manual (UM2198 rev.4, table 50) shows that MFX has three unused pins: 10,11,12.
How to connect to these pins? I cannot find a connector on the schema in UM2198.
On the schema, Fig. 59 all these MFX pins are connected to something. Are they really free to use?