STM32H7A3: SPI not working if SCK disabled
I am trying to emit data on SPI MOSI without enabling the corresponding SCK pin. This is useful for instance to control WS2812-type LEDs.
β
However when I use `HAL_SPI_Transmit_IT` to transfer 3 words, the IRQ Handler gets called 3 times (triggered by a TXP event) but then it doesn't get called the 4th time because the EOT flag in SPI_SR is never raised. In other words the transfer doesn't finish. Similarly, a transfer started with `HAL_SPI_Transmit_DMA` will also not complete.
β
When I put any of the corresponding SCK GPIOβs (that exist on the package) into SPI alternate function mode, the transfer completes normally.
β
On the STM32F722 the SPI works fine without SCK pin.
β
Is this expected behavior on the STM32H7A3? The reference manual (Figure 579) suggests some entanglement between SPI core and SCK pin but I didn't find a clear statement that SCK must be enabled.
β
Below is the code that I was using for the experiments. "Works" means that the variable `works` is incremented. "Doesn't work" means that the variable `works` remains zero and the CPU spins on line 185.
#include "main.h"
//// works ////
//#define SPI SPI1
//#define SCK_PORT GPIOA
//#define SCK_PIN GPIO_PIN_5
//// works ////
//#define SPI SPI1
//#define SCK_PORT GPIOB
//#define SCK_PIN GPIO_PIN_3
//// doesn't work (pin not available on package) ////
//#define SPI SPI1
//#define SCK_PORT GPIOG
//#define SCK_PIN GPIO_PIN_11
//// works ////
//#define SPI SPI2
//#define SCK_PORT GPIOA
//#define SCK_PIN GPIO_PIN_9
//// works ////
//#define SPI SPI2
//#define SCK_PORT GPIOA
//#define SCK_PIN GPIO_PIN_12
//// can't verify ////
//#define SPI SPI2
//#define SCK_PORT GPIOB
//#define SCK_PIN GPIO_PIN_10
//// works ////
//#define SPI SPI2
//#define SCK_PORT GPIOB
//#define SCK_PIN GPIO_PIN_13
//// doesn't work (pin not available on package) ////
//#define SPI SPI2
//#define SCK_PORT GPIOD
//#define SCK_PIN GPIO_PIN_3
//// doesn't work (pin not available on package) ////
//#define SPI SPI2
//#define SCK_PORT GPIOI
//#define SCK_PIN GPIO_PIN_1
//// works ////
//#define SPI SPI3
//#define SCK_PORT GPIOB
//#define SCK_PIN GPIO_PIN_3
//// works ////
//#define SPI SPI3
//#define SCK_PORT GPIOC
//#define SCK_PIN GPIO_PIN_10
//// doesn't work ////
//#define SPI SPI1
//#define NO_SCK
//// doesn't work ////
//#define SPI SPI2
//#define NO_SCK
//// doesn't work ////
//#define SPI SPI3
//#define NO_SCK
SPI_HandleTypeDef hspi;
void SystemClock_Config(void);
int main(void) {
HAL_Init();
__HAL_RCC_SYSCFG_CLK_ENABLE();
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 35;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK) {
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SPI1 | RCC_PERIPHCLK_SPI2 | RCC_PERIPHCLK_SPI3;
PeriphClkInitStruct.Spi123ClockSelection = RCC_SPI123CLKSOURCE_PLL;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK) {
Error_Handler();
}
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOG_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOI_CLK_ENABLE();
__HAL_RCC_SPI1_CLK_ENABLE();
__HAL_RCC_SPI2_CLK_ENABLE();
__HAL_RCC_SPI3_CLK_ENABLE();
HAL_NVIC_SetPriority(SPI1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI1_IRQn);
HAL_NVIC_SetPriority(SPI2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI2_IRQn);
HAL_NVIC_SetPriority(SPI3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SPI3_IRQn);
hspi.Instance = SPI;
hspi.Init.Mode = SPI_MODE_MASTER;
hspi.Init.Direction = SPI_DIRECTION_2LINES;
hspi.Init.DataSize = SPI_DATASIZE_16BIT;
hspi.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi.Init.NSS = SPI_NSS_SOFT;
hspi.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
hspi.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi.Init.TIMode = SPI_TIMODE_DISABLE;
hspi.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi.Init.CRCPolynomial = 0x0;
hspi.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
hspi.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
hspi.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
hspi.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
hspi.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
hspi.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
hspi.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
hspi.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
hspi.Init.IOSwap = SPI_IO_SWAP_DISABLE;
if (HAL_SPI_Init(&hspi) != HAL_OK) {
Error_Handler();
}
#ifndef NO_SCK
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = SCK_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = (SPI == SPI1) ? GPIO_AF5_SPI1 :
(SPI == SPI2) ? GPIO_AF5_SPI2 :
GPIO_AF6_SPI3;
HAL_GPIO_Init(SCK_PORT, &GPIO_InitStruct);
#endif
volatile int works = 0;
while (1) {
uint16_t data[] = {0xffff, 0xffff, 0xffff};
HAL_SPI_Transmit_IT(&hspi, (uint8_t*)data, 3);
while (hspi.State != HAL_SPI_STATE_READY);
works++;
}
}
void Error_Handler(void) {
for(;;);
}
void SysTick_Handler(void) {
HAL_IncTick();
}
void SPI1_IRQHandler(void) {
HAL_SPI_IRQHandler(&hspi);
}
void SPI2_IRQHandler(void) {
HAL_SPI_IRQHandler(&hspi);
}
void SPI3_IRQHandler(void) {
HAL_SPI_IRQHandler(&hspi);
}β