Skip to main content
KVeer.1
Associate
April 14, 2020
Question

STM32F446RE ADC not triggered via TIM1 in injected mode

  • April 14, 2020
  • 0 replies
  • 497 views

Hello all,

I am trying to configure an ADC in injected mode via a trigger from TIMER 1. I want to trigger ADC whenever the timer RESETS. For this, I have set the TIM1's master mode to generate ADC trigger signal during timer RESET. I have configured ADC in injected mode to trigger for the same and have also set the ADC interrupt in trigger mode.

However, I found that it doesnot trigger for whatever reason. I have attached my ADC initialization code for you guys to take a look. Could you tell me where I'm going wrong?

#define ADCbase_ADDR (uint32_t)0x40012000
#define ADC1 0x00
#define ADC2 0x100
#define ADC3 0x200
 
#define ADC1base_ADDR (ADCbase_ADDR + ADC1)
#define ADC2base_ADDR (ADCbase_ADDR + ADC2)
#define ADC3base_ADDR (ADCbase_ADDR + ADC3)
 
//Register Offsets
#define ADC_SR 0x00
#define ADC_CR1 0x04
#define ADC_CR2 0x08
#define ADC_SMPR1 0x0C
#define ADC_SMPR2 0x10
#define ADC_JOFR1 0x14
#define ADC_JOFR2 0x18
#define ADC_JOFR3 0x1C
#define ADC_JOFR4 0x20
#define ADC_HTR 0x24
#define ADC_LTR 0x28
#define ADC_SQR1 0x2C
#define ADC_SQR2 0x30
#define ADC_SQR3 0x34
#define ADC_JSQR 0x38
#define ADC_JDR1 0x3C
#define ADC_JDR2 0x40
#define ADC_JDR3 0x44
#define ADC_JDR4 0x48
#define ADC_DR 0x4C
 
//RCC Registers
#define RCC_Base_Address (uint32_t)0x40023800
#define RCC_APB2ENR 0x44
#define AHB1_ENR 0x30
 
#define ADC1Clock_Enable_BIT (uint32_t)(1<<8)
#define ADC_ENABLE_BIT 0x00000001
#define GPIOA_RCC_Enable_Bit 0x00000001
 
#define GPIOA_Base_ADDR 0x40020000
#define GPIOB_Base_ADDR 0x40020400
#define GPIOC_Base_ADDR 0x40020800
 
#define GPIOA_MODER 0x00
 
//GPIO Registers
#define AN0 (0x00000003)
#define Timer1_TRGO_bits 0x00010000 //bits 16 through 19
#define Trigger_Rising 0x00300000
 
//Timer Registers
#define TMR1_BASE_ADDR 0x40010000
#define TIMx_CR2 0x04
 
#define MMS_BITS_RESET_MODE 0x00000070
 
uint32_t *p; //pointer pointing to the address of registers
//configure
 
 
void ADC_Init(void)
{
	//enable GPIO port A's peripheral clock on AHB1
	p = (uint32_t)(RCC_Base_Address + AHB1_ENR);
	*p = (*p | GPIOA_RCC_Enable_Bit);
	//enable ADC1's peripheral clock on APB2
	p = (uint32_t)(RCC_Base_Address + RCC_APB2ENR);
	*p = (*p | ADC1Clock_Enable_BIT);
 
	//configure PA0 as analog input
	p = (uint32_t)(GPIOA_Base_ADDR + GPIOA_MODER);
	*p = (*p | AN0);
 
 //Enable interrupt for injected channels
	p = (uint32_t)(ADC1base_ADDR + ADC_CR1);
	*p = 0x00000000;
	*p = *p |((uint32_t)(1<<7));
 
	//point to CR2
	p = (uint32_t)(ADC1base_ADDR + ADC_CR2);
	*p = 0x00000000;
	//External event select for injected group for rising edge
	*p = *p |(Trigger_Rising);
 
	//Select Timer 1 TRGO as the SOC trigger source
	*p = *p |(Timer1_TRGO_bits);
	//Implied Settings by CR2 Reset
	//DMA disabled
	//The EOC bit is set at the end of each sequence of regular conversions. Overrun detection is enabled only if DMA=1.
	//Data Right alignment
	//SIngle Conversion Mode
	//ADC conversion disabled
 
	//Timer1 Master Mode selection for configuring TRGO conditions
	p = (uint32_t)(TMR1_BASE_ADDR + TIMx_CR2);
	*p = *p & ~(MMS_BITS_RESET_MODE);
 
	//switch to injected sequence register
	p = (uint32_t)(ADC1base_ADDR + ADC_JSQR);
	*p = 0x00000000;
	//implied changes:
	//one conversion
	//connect first conversion in injected sequence as channel 1
	*p = *p|(0x00000000); //selecting channel 0 as the analog input
 
 //turn on ADC1
	p = (uint32_t)(ADC1base_ADDR + ADC_CR2);
	*p = *p |((uint32_t)(ADC_ENABLE_BIT));
}
 
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
 //UNUSED(hadc);
	HAL_GPIO_TogglePin(GPIOB, test_Pin);
 
//This is not getting triggered!!
}

This topic has been closed for replies.