Question
STM32F042F6- TSSOP20- Where is the TIMER 2 Channel 1?
Posted on November 01, 2016 at 17:28
Dear all experts,
I am programming Incremental Encoder Reading project for 2 encoders.I intend to use TIM2, and TIM3 for Encoder Config with 4X Reading. I check the datasheet (DM00105814) for MCU Pin configuration.For TIM3, I can see TIM3-CH1, and TIM3_CH2 are Pin PA6, PA7For TIM2, I cannot find TIM2-CH1, instead of that, I see 2 pin PA0 and PA5 can config to same function TIM2-CH1-ETR.As subject, Could any one can help me to find out TIM2-CH1?Thank you in advance.