Skip to main content
javanzee
Visitor II
February 5, 2013
Question

STM32F0 Discovery JP1 (STLINK USART RX,TX)

  • February 5, 2013
  • 0 replies
  • 426 views
Posted on February 05, 2013 at 01:35

What is the purpose of JP1?  It connects to the STLINK MCU, and via two solder-jumpers on the bottom of the board (SB14,15) to PA9,10 of the 'F051 (the USART-1 pins).  Can the STLINK enumerate as a CDC endpoint, and thus provide a serial port for the 'F0?  Or, perhaps it is there to explore the built-in hardware bootloader (again enumerated as a CDC endpoint)? If either of these speculations is true, would the STLINK MCU first need to be re-programmed as a CDC device via the DFU loader?

    This topic has been closed for replies.