STM32Cube_FW_F2_V1.4.0\Projects\STM32F207ZG-Nucleo\Examples\UART\UART_Printf , printing garbage data over the terminal
Hi,
I am flashing the UART sample code given in STM32CubeF2 in my STM32F207ZG nucleo board,
It is compiling and flashing well but when I see the output on terminal (Tera term) it is printing garbage data (few characters are matching).
I have seen the baude rate in example is 9600 so a have set the same on tera term as well.
i should get o/p as:-
UART Printf Example: retarget the C library printf function to the UART
** Test finished successfully. **
And what I am getting is-
Õ�RT �òénôæ Eøampìåº òåôaògåô ôhå C ìébòaòy pòénôæ æunãôéïn ôï ôhå Õ�RT
** Tåsô æénéshåd suããåssæuììy® **