Question
STM23L031F6P6‘s UART don't work after resume from STOP mode with RTC
It's my first time to use STM23L031F6P6,and i got some troubles
both UART2 & LPUART1 don't work after resume from STOP mode
is there somebody can help me?
main code shows below:
void test1(void)
{
HAL_Init();
RTC_Config();
while(1)
{
SystemClock_Config();
init();
printf("------- wake up --------\r\n");
LedOn(1);
HAL_Delay(5000);
LedOff(1);
HAL_Delay(5000);
printf("\r\n------- sleep --------\r\n");
rtc_wakeup_cfg();
SystemPower_Config();
HW_WakeupPinInit();
enter_stop_mode();
}
}
void rtc_wakeup_cfg(void)
{
HAL_RTCEx_DeactivateWakeUpTimer(&RTCHandle);
HAL_RTCEx_SetWakeUpTimer_IT(&RTCHandle, RTC_TIME,
RTC_WAKEUPCLOCK_CK_SPRE_16BITS);
}
void enter_stop_mode(void)
{
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
}
void HW_WakeupPinInit(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_6 | GPIO_PIN_7;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
__HAL_RCC_GPIOA_CLK_ENABLE();
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_13 | GPIO_PIN_14;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
NVIC_SetPriority((IRQn_Type)(EXTI4_15_IRQn), 0x03);
HAL_NVIC_EnableIRQ((IRQn_Type)(EXTI4_15_IRQn));
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInit;
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_4;
RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_LPUART1;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
static void SystemPower_Config(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableUltraLowPower();
HAL_PWREx_EnableFastWakeUp();
__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI);
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
GPIO_InitStructure.Pin = GPIO_PIN_All;
GPIO_InitStructure.Mode = GPIO_MODE_ANALOG;
GPIO_InitStructure.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOH, &GPIO_InitStructure);
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
}
static void RTC_Config(void)
{
RTCHandle.Instance = RTC;
RTCHandle.Init.HourFormat = RTC_HOURFORMAT_24;
RTCHandle.Init.AsynchPrediv = RTC_ASYNCH_PREDIV;
RTCHandle.Init.SynchPrediv = RTC_SYNCH_PREDIV;
RTCHandle.Init.OutPut = RTC_OUTPUT_DISABLE;
RTCHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
RTCHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if(HAL_RTC_Init(&RTCHandle) != HAL_OK)
{
Error_Handler();
}
}
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
GPIOA->MODER = 0xFFFFFFFF;
GPIOB->MODER = 0xFFFFFFFF;
GPIOC->MODER = 0xFFFFFFFF;
GPIOH->MODER = 0xFFFFFFFF;
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4|GPIO_PIN_5, GPIO_PIN_SET);
GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_4|GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
HAL_NVIC_SetPriority(EXTI4_15_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI4_15_IRQn);
}
void MX_DMA_Init(void)
{
__HAL_RCC_DMA1_CLK_ENABLE();
HAL_NVIC_SetPriority(DMA1_Channel2_3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);
}
void MX_LPUART1_UART_Init(void)
{
hlpuart1.Instance = LPUART1;
hlpuart1.Init.BaudRate = 115200;
hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
hlpuart1.Init.StopBits = UART_STOPBITS_1;
hlpuart1.Init.Parity = UART_PARITY_NONE;
hlpuart1.Init.Mode = UART_MODE_TX_RX;
hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&hlpuart1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
void MX_USART2_UART_Init(void)
{
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{
GPIO_InitTypeDef GPIO_InitStruct;
if(huart->Instance==LPUART1)
{
__HAL_RCC_LPUART1_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF6_LPUART1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
hdma_lpuart1_rx.Instance = DMA1_Channel3;
hdma_lpuart1_rx.Init.Request = DMA_REQUEST_5;
hdma_lpuart1_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_lpuart1_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_lpuart1_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_lpuart1_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_lpuart1_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_lpuart1_rx.Init.Mode = DMA_NORMAL;
hdma_lpuart1_rx.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_lpuart1_rx) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
__HAL_LINKDMA(huart,hdmarx,hdma_lpuart1_rx);
HAL_NVIC_SetPriority(AES_RNG_LPUART1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(AES_RNG_LPUART1_IRQn);
}
else if(huart->Instance==USART2)
{
__HAL_RCC_USART2_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_USART2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
HAL_NVIC_SetPriority(USART2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART2_IRQn);
}
}
void HAL_UART_MspDeInit(UART_HandleTypeDef* huart)
{
if(huart->Instance==LPUART1)
{
__HAL_RCC_LPUART1_CLK_DISABLE();
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_2|GPIO_PIN_3);
HAL_DMA_DeInit(huart->hdmarx);
HAL_NVIC_DisableIRQ(AES_RNG_LPUART1_IRQn);
}
else if(huart->Instance==USART2)
{
__HAL_RCC_USART2_CLK_DISABLE();
HAL_GPIO_DeInit(GPIOA, GPIO_PIN_9|GPIO_PIN_10);
HAL_NVIC_DisableIRQ(USART2_IRQn);
}
}
void EnableUartIT(void)//′??ú3?ê??ˉ
{
__HAL_UART_ENABLE_IT(&hlpuart1, UART_IT_IDLE);
__HAL_UART_CLEAR_IDLEFLAG(&hlpuart1); HAL_UART_Receive_DMA(&hlpuart1,LPUart1type.LPUart1DMARecBuff,LPUART1_DMA_REC_SIZE);
__HAL_UART_ENABLE_IT(&huart2, UART_IT_RXNE);
HAL_UART_Receive_IT(&huart2, &Usart2Rx, 1);
}